Other Parts Discussed in Thread: TMS320C6678
Hi,
The SPRS691d datasheet gives p.214 some timing informations about the hyperlink sideband signals. The clocks frequency are identified as C1,C2,C3,C4 with a value of 6.4ns. But this is not clear at all if this value is a minimum, typical, maximum or a programmable (although I could not find any register for that purpose in the SPRUGW8A).
Could you clarify that characteristic please ?
6.4ns (if correct) corresponds to a 156.25MHz frequency which seems to be oversized if we consider that only some bytes need to be transmitted.
The problem is that IBIS simulations we did at MCMTXPMCLK=156.25MHz (TMS320C6678_4_2_1_R1P5B_BC1850CGHYPBFB_DRIVER_MODE model) over a 5cm trace length demonstrates that in the low corner case, the clock high level does not even reach 1.5V. Such a high frequency does not seem to be apropriate. Do you confirm, or is there a mistake in the datasheet ?
Thank you for your help,
with best regards,
Bruno