This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

how can re-flash NAND on evm8168

Hi folks,

I was flashing the nand of the evm8168 board en the boot file I flashed is not the correct, I put it in hex dir 0x00. The current went off and the flash stopped.

Now when I want to reflash de nand this message appears:

IcePick_D_0: Error connecting to the target: (Error -501 @ 0x0) The built-in scan-path length measurement failed. The built-in scan-path reliability tests cannot be performed without knowledge of the scan-path length. Try specifying the scan-path lengths in the command-line options or board configuration file of this utility or debugger. (Emulation package 5.0.872.0)

What can I do to re-flash de nand? Can I flash it with another methor instead of using CCSv5.3?

It is very urgent.

Thanks in advance,

Regards,

Inigo