Other Parts Discussed in Thread: OMAPL138
Have ther been any updates to the ROM MMC IP for the OMAP138 to allow it to fully support eMMC v4.41 yet?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OMAPL138
Have ther been any updates to the ROM MMC IP for the OMAP138 to allow it to fully support eMMC v4.41 yet?
Hi Dwight
No plans to upgrade the OMAPL138 RBL to support eMMC v4.41.
The RBL support for MMC/SD including eMMC is as stated in the boot loader application note
The MMC/SD boot mode is compliant with version 2.0 of the SD specification and version 4.2 of the
eMMC specification. The boot loader and MMC/SD peripheral does not support features of the eMMC 4.3
or 4.4 specifications related to boot (no boot operation mode and no support for boot partitions). The AIS
boot image is expected to be in the user data area of the memory device, written to address 0 of that
region. The bootloader detects the AIS image by checking for the magic word (0x41504954). If the magic
word is not found, the bootloader increments the starting address by 0x200 and tries again. The
bootloader fails if the magic word is not found within the first 2 MB of the memory card.
Regards
Mukul