Other Parts Discussed in Thread: OMAP-L138
Hi there,
could anybody help me? i'll highly appreciate it.
i just got a TMDXLCDK138, am following the start guide, and got error warning as in below. any suggestion pls to fix it? i'll highly appreciate it.
NAND: 512 MiB
MMC: davinci: 0
Bad block table found at page 262080, version 0x01
Bad block table found at page 262016, version 0x01
*** Warning - bad CRC, using default environment
In: serial
Out: serial
Err: serial
ARM Clock : 456000000 Hz
DDR Clock : 150000000 Hz
Net: Ethernet PHY: GENERIC @ 0x07
DaVinci-EMAC Hit any key to stop autoboot: 0
Card did not respond to voltage select!
Unknown command 'sf' - try 'help'
Unknown command 'sf' - try 'help'
Wrong Image Format for bootm command
ERROR: can't get kernel image!
U-Boot >