This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365 NAND boot ECC error

Hello,

I am facing DM365 NAND boot error problem.

Detail:
Function:DEVICE_NAND_ECC_correct functio() detect error when NANDERRADD1 value is small.

 addOffset = 519 - (AEMIF->NANDERRADD1 & (0x000003FF));
 addOffset>511 --->error! 

What does this error mean?
(Error of spare byte?)

FYI:
User program code in NAND can be read correctly in this case.
(I verified the code as binary data.)

Regards,

  • Yoichi-san,

    The issue is that data is present only up to 512 bytes and anything beyond that is spare area. So, if there is an error in spare area. then its something that cannot be handled by the function. But this should not happen in normal case. There might be something else that's going wrong which is triggering this. 

  • Dear Renjith Thomas,

    Thank you for your reply.

    > There might be something else that's going wrong which is triggering this.
    Do you know any cause which is triggering this?
    (How can I avoid this issue?)

    Regards,

  • Dear Yoichi-san,

    Its difficult to comment now on what could be the exact problem. Need to see the logic that's implemented. Will you be able upload the source file?

  • Dear Renjith Thomas,

    I have attached the source file, device_nand.c.
    (The error is detected as  "return E_FAIL".)

    device_nand.c line 287:

      switch( numE ){
       case 3:     // Four errors
        addOffset = 519 - ( (AEMIF->NANDERRADD2 & (0x03FF0000))>>16 );
        if (addOffset > 511) return E_FAIL;
        corrValue = (AEMIF->NANDERRVAL2 & (0x03FF0000))>>16;
        data[addOffset] ^= (Uint8)corrValue;
        // Fall through to case 2
       case 2:     // Three errors
        addOffset = 519 - (AEMIF->NANDERRADD2 & (0x000003FF));
        if (addOffset > 511) return E_FAIL;
        corrValue = AEMIF->NANDERRVAL2 & (0x000003FF);
        data[addOffset] ^= (Uint8)corrValue;
        // Fall through to case 1
       case 1:     // Two errors
        addOffset = 519 - ( (AEMIF->NANDERRADD1 & (0x03FF0000))>>16 );
        if (addOffset > 511) return E_FAIL;
        corrValue = (AEMIF->NANDERRVAL1 & (0x03FF0000))>>16;
        data[addOffset] ^= (Uint8)corrValue;
        // Fall through to case 0
       case 0:     // One error
        addOffset = 519 - (AEMIF->NANDERRADD1 & (0x000003FF));
        if (addOffset > 511) return E_FAIL;
        corrValue = AEMIF->NANDERRVAL1 & (0x3FF);
        data[addOffset] ^= (Uint8)corrValue;
        break;
      }

    Also, I have another question.

    The source code makes check adr as follows:
        addOffset = 519 - ( (AEMIF->NANDERRADD2 & (0x03FF0000))>>16 );

    I want to know the meaning of the "519".
    I suppose 519=512+7.

    Description from TMS320DM36x Digital Media System-on-Chip (DMSoC) Asynchronous External Memory Interface (EMIF) User's Guide(SPRUFI1C):
        2.5.6.6.2 4-Bit ECC
        Read the error address from the NAND Flash Error Address 1-2 registers (NANDERRADD[2:1]).
        Address for the errored word is equal to (total_words_read + 7 - address_value).

    But I cannot understand the meaning of "+7".

    Regards,

    /* --------------------------------------------------------------------------
      FILE        : device_nand.c
      PROJECT     : TI Booting and Flashing Utilities
      AUTHOR      : Daniel Allred
      DESC        : This file descibes and implements various device-specific NAND
                    functionality.
    -------------------------------------------------------------------------- */
    
    // General type include
    #include "tistdtypes.h"
    
    // Device specific CSL
    #include "device.h"
    
    // Device specific NAND details
    #include "device_nand.h"
    
    // Generic NAND header file
    #include "nand.h"
    
    
    /************************************************************
    * Explicit External Declarations                            *
    ************************************************************/
    
    
    /************************************************************
    * Local Macro Declarations                                  *
    ************************************************************/
    
    // ECC offset defines
    #define DEVICE_NAND_ECC_START_OFFSET (6)
    
    
    /************************************************************
    * Local Function Declarations                               *
    ************************************************************/
    
    // Required implementation for NAND_ECC_Info struct
    static void DEVICE_NAND_ECC_calculate(NAND_InfoHandle hNandInfo, Uint8 *data, Uint8 *calcECC);
    static void DEVICE_NAND_ECC_store(NAND_InfoHandle hNandInfo, Uint8 *spareBytes, Uint8 opNum, Uint8 *calcECC);
    static void DEVICE_NAND_ECC_enable(NAND_InfoHandle hNandInfo);
    static void DEVICE_NAND_ECC_disable(NAND_InfoHandle hNandInfo);
    static void DEVICE_NAND_ECC_read(NAND_InfoHandle hNandInfo, Uint8 *spareBytes, Uint8 opNum, Uint8 *readECC);
    static Uint32 DEVICE_NAND_ECC_correct(NAND_InfoHandle hNandInfo, Uint8 *data, Uint8 *readECC);
    
    // Required implementation for NAND_BB_Info struct
    static void DEVICE_NAND_BB_markSpareBytes(NAND_InfoHandle hNandInfo, Uint8 *spareBytes);
    static Uint32 DEVICE_NAND_BB_checkSpareBytes(NAND_InfoHandle hNandInfo, Uint8 *spareBytes);
    
    
    /************************************************************
    * Local Variable Definitions                                *
    ************************************************************/
    
    
    /************************************************************
    * Global Variable Definitions                               *
    ************************************************************/
    
    // Specfic ECC info to support ROM of device
    const NAND_ECC_InfoObj DEVICE_NAND_ECC_info =
    {
    	TRUE,         // ECCEnable
    	16,           // calcECCByteCnt
    	10,           // storedECCByteCnt
    	&(DEVICE_NAND_ECC_calculate),
    	&(DEVICE_NAND_ECC_store),
    	&(DEVICE_NAND_ECC_enable),
    	&(DEVICE_NAND_ECC_disable),
    	&(DEVICE_NAND_ECC_read),
    	&(DEVICE_NAND_ECC_correct)
    };
    
    const NAND_BB_InfoObj DEVICE_NAND_BB_info =
    {
    	TRUE,
    	TRUE,
    	&(DEVICE_NAND_BB_markSpareBytes),
    	&(DEVICE_NAND_BB_checkSpareBytes)
    };
    
    // Specific Page layout to support ROM of device
    const NAND_PAGE_LayoutObj DEVICE_NAND_PAGE_layout =
    {
    	// Data region definition
    	{
    		NAND_REGION_DATA,					// Region Type
    		NAND_OFFSETS_RELTODATA,				// Offsets relative type
    		DEVICE_NAND_MAX_BYTES_PER_OP,		// bytesPerOp
    		{0*(512) ,1*(512) ,2*(512) ,3*(512) ,	// dataOffsets
    		 4*(512) ,5*(512) ,6*(512) ,7*(512) ,
    		 8*(512) ,9*(512) ,10*(512),11*(512),
    		 12*(512),13*(512),14*(512),15*(512)
    
    		}
    	},
    
    	// Spare region definition
    	{
    		NAND_REGION_SPARE,					// Region Type
    		NAND_OFFSETS_RELTOSPARE,			// Offsets relative type
    		DEVICE_NAND_MAX_SPAREBYTES_PER_OP,	// bytesPerOp
    		{0*16  ,1*16  ,2*16  ,3*16  ,			// spareOffsets
    		 4*16  ,5*16  ,6*16  ,7*16  ,
    		 8*16  ,9*16  ,10*16 ,11*16 ,
    		 12*16 ,13*16 ,14*16 ,15*16
    
    		}
    	}
    };
    
    //FOR DM365,referred DM365 ROM code
    const NAND_CHIP_InfoObj DEVICE_NAND_CHIP_infoTable[] =
    {
    	{ 0xE3,   512,        16,             512+16},	// 4 MB
    	{ 0xE5,   512,        16,             512+16},	// 4 MB
    	{ 0xE6,   1024,       16,             512+16},	// 8 MB
    	{ 0x39,   1024,       16,             512+16},	// 8 MB
    	{ 0x6B,   1024,       16,             512+16},	// 8 MB
    	{ 0x73,   1024,       32,             512+16},	// 16 MB
    	{ 0x33,   1024,       32,             512+16},	// 16 MB
    	{ 0x75,   2048,       32,             512+16},	// 32 MB
    	{ 0x35,   2048,       32,             512+16},	// 32 MB
    	{ 0x76,   4096,       32,             512+16},	// 64 MB
    	{ 0x36,   4096,       32,             512+16},	// 64 MB
    	{ 0x79,   8192,       32,             512+16},	// 128 MB
    	{ 0x71,   16384,      32,             512+16},	// 256 MB
    	{ 0x46,   4096,       32,             512+16},  // 64 MB
    	{ 0x56,   4096,       32,             512+16},  // 64 MB
    	{ 0x74,   8192,       32,             512+16},  // 128 MB
    	{ 0xF1,   1024,       64,             2048+64}, // 128 MB
    	{ 0xA1,   1024,       64,             2048+64},	// 128 MB
    	{ 0xAA,   2048,       64,             2048+64},	// 256 MB (4th ID byte will be checked)
    	{ 0xDA,   2048,       64,             2048+64},	// 256 MB (4th ID byte will be checked)
    	{ 0xAC,   4096,       64,             2048+64}, // 512 MB (4th ID byte will be checked)
    	{ 0xDC,   4096,       64,             2048+64},	// 512 MB (4th ID byte will be checked)
    	{ 0xB1,   1024,       64,             2048+64}, // 128 MB
    	{ 0xC1,   1024,       64,             2048+64}, // 128 MB
    	{ 0xD3,   8192,       64,             2048+64}, // 1 GB
    	{ 0xD5,   8192,       64,             4096+128}, // 2 GB
    	{ 0x00,   0,          0,              0}	      // Dummy null entry to indicate end of table
    
    };
    
    
    /************************************************************
    * Global Function Definitions                               *
    ************************************************************/
    
    static void DEVICE_NAND_ECC_calculate(NAND_InfoHandle hNandInfo, Uint8 *data, Uint8 *calcECC)
    {
    	Uint32		*eccValue = (Uint32 *) calcECC;
    	eccValue[0] = (AEMIF->NAND4BITECC1 & 0x03FF03FF);
    	eccValue[1] = (AEMIF->NAND4BITECC2 & 0x03FF03FF);
    	eccValue[2] = (AEMIF->NAND4BITECC3 & 0x03FF03FF);
    	eccValue[3] = (AEMIF->NAND4BITECC4 & 0x03FF03FF);
    }
    
    // Do conversion from 8 10-bit ECC values from HW (in 16 byte input) to 10 8-bit continguous values for storage in spare bytes
    static void DEVICE_NAND_ECC_store(NAND_InfoHandle hNandInfo, Uint8 *spareBytes, Uint8 opNum, Uint8 *calcECC)
    {
    	Uint32		out[3], in[4], i;
    
    	for (i=0; i <DEVICE_NAND_ECC_info.calcECCByteCnt; i++){
    		((Uint8 *)in)[i] = ((Uint8 *)calcECC)[i];
    	}
    
    	out[0] = ((in[1]&0x00030000) <<14) | ((in[1]&0x000003FF) <<20) |
    			 ((in[0]&0x03FF0000) >> 6) | ((in[0]&0x000003FF)     );
    	out[1] = ((in[3]&0x0000000F) <<28) | ((in[2]&0x03FF0000) << 2) |
    			 ((in[2]&0x000003FF) << 8) | ((in[1]&0x03FC0000) >>18);
    	out[2] = ((out[2]&0xFFFF0000)    ) | ((in[3]&0x03FF0000) >>10) |
    			 ((in[3]&0x000003F0) >> 4);
    
    	for (i=0; i <DEVICE_NAND_ECC_info.storedECCByteCnt; i++){
    		spareBytes[i + DEVICE_NAND_ECC_START_OFFSET + hNandInfo->spareBytesPerOp*opNum] = ((Uint8 *)out)[i];
    	}
    }
    
    static void DEVICE_NAND_ECC_enable(NAND_InfoHandle hNandInfo)
    {
    	// Write appropriate bit to start ECC calcualtions (bit 12 for four bit ECC)
    	AEMIF->NANDFCR |= 0x1<<DEVICE_EMIF_NANFCR_4BITECC_START_SHIFT;
    }
    
    static void DEVICE_NAND_ECC_disable(NAND_InfoHandle hNandInfo)
    {
    	VUint32		dummy;
    
    	// Read any ECC register to end the calculation and clear the ECC start bit
    	dummy = AEMIF->NAND4BITECC1;
    }
    
    // Read 10 8-bit values from pagebuffer and convert to 8 10-bit values
    static void DEVICE_NAND_ECC_read(NAND_InfoHandle hNandInfo, Uint8 *spareBytes, Uint8 opNum, Uint8 *readECC)
    {
    	Uint32		in[3], out[4], i;
    
    	for (i=0; i <DEVICE_NAND_ECC_info.storedECCByteCnt; i++){
    		((Uint8 *)in)[i] = spareBytes[i + DEVICE_NAND_ECC_START_OFFSET + hNandInfo->spareBytesPerOp*opNum];
    	}
    
    	out[0] = ((in[0]&0x000FFC00) << 6) | ((in[0]&0x000003FF)     );
    	out[1] = ((in[1]&0x000000FF) <<18) | ((in[0]&0xC0000000) >>14) |
    			 ((in[0]&0x3FF00000) >>20);
    	out[2] = ((in[1]&0x0FFC0000) >> 2) | ((in[1]&0x0003FF00) >> 8);
    	out[3] = ((in[2]&0x0000FFC0) <<10) | ((in[2]&0x0000003F) << 4) |
    			 ((in[1]&0xF0000000) >>28);
    
    	for (i=0; i <DEVICE_NAND_ECC_info.calcECCByteCnt; i++){
    		readECC[i] = ((Uint8 *)out)[i];
    	}
    }
    
    static Uint32 DEVICE_NAND_ECC_correct(NAND_InfoHandle hNandInfo, Uint8 *data, Uint8 *readECC)
    {
    	VUint32		temp, corrState, numE;
    	Uint32		i;
    	Uint32		ix;		// ois
    	Uint16		addOffset, corrValue;
    	Uint16		*syndrome10 = (Uint16 *)readECC;
    
    	// Clear bit13 of NANDFCR
    	temp = AEMIF->NANDERRADD1;
    
    	// Load the syndrome10 (from 7 to 0) values
    	for(i=8;i>0;i--)	{
    		AEMIF->NAND4BITECCLOAD = (syndrome10[i-1] & 0x000003FF);
    	}
    
    	// Read the EMIF status and version (dummy call)
    	temp = AEMIF->ERCSR;
    
    	// Check if error is detected
    	temp = (AEMIF->NAND4BITECC1 & 0x03FF03FF) | (AEMIF->NAND4BITECC2 & 0x03FF03FF) |
    		   (AEMIF->NAND4BITECC3 & 0x03FF03FF) | (AEMIF->NAND4BITECC4 & 0x03FF03FF);
    	if(temp == 0){
    		return E_PASS;
    	}
    
    	// Start calcuating the correction addresses and values
    	AEMIF->NANDFCR |= (0x1U << DEVICE_EMIF_NANFCR_4BITECC_ADD_CALC_START_SHIFT);
    
    #if 1	// ois
    	// wait for the ECC calculations are complete, or timeout
    	for(i = NAND_TIMEOUT; i > 0; i--){
    		temp = (AEMIF->NANDFSR & DEVICE_EMIF_NANDFSR_ECC_STATE_MASK) >> DEVICE_EMIF_NANDFSR_ECC_STATE_SHIFT;
    		if(temp > 3){				// not complete
    			continue;
    		}
    		for(ix = 0; ix < 1024; ix++){
    			// wait few
    		}
    		// Re-read correction state
    		corrState = (AEMIF->NANDFSR & DEVICE_EMIF_NANDFSR_ECC_STATE_MASK) >> DEVICE_EMIF_NANDFSR_ECC_STATE_SHIFT;
    		if(corrState != temp){		// unmatch
    			continue;
    		}
    	}
    #else
    	// Loop until timeout or the ECC calculations are complete (bit 11:10 == 00b)
    	i = NAND_TIMEOUT;
    	do {
    		temp = (AEMIF->NANDFSR & DEVICE_EMIF_NANDFSR_ECC_STATE_MASK)>>10;
    		i--;
    	}
    	while((i>0) && (temp != 0x0));
    
    	// Read final correction state (should be 0x0, 0x1, 0x2, or 0x3)
    	corrState = (AEMIF->NANDFSR & DEVICE_EMIF_NANDFSR_ECC_STATE_MASK) >> DEVICE_EMIF_NANDFSR_ECC_STATE_SHIFT;
    #endif
    
    	if ((corrState == 1) || (corrState > 3)){
    		temp = AEMIF->NANDERRADD1;
    		return E_FAIL;
    	}
    	else if (corrState == 0){
    		temp = AEMIF->NANDERRADD1;
    		return E_PASS;
    	}
    	else{
    		// Error detected and address calculated
    		// Number of errors corrected 17:16
    		numE = (AEMIF->NANDFSR & DEVICE_EMIF_NANDFSR_ECC_ERRNUM_MASK) >> DEVICE_EMIF_NANDFSR_ECC_ERRNUM_SHIFT;
    
    		switch( numE ){
    			case 3:     // Four errors
    				addOffset = 519 - ( (AEMIF->NANDERRADD2 & (0x03FF0000))>>16 );
    				if (addOffset > 511) return E_FAIL;
    				corrValue = (AEMIF->NANDERRVAL2 & (0x03FF0000))>>16;
    				data[addOffset] ^= (Uint8)corrValue;
    				// Fall through to case 2
    			case 2:     // Three errors
    				addOffset = 519 - (AEMIF->NANDERRADD2 & (0x000003FF));
    				if (addOffset > 511) return E_FAIL;
    				corrValue = AEMIF->NANDERRVAL2 & (0x000003FF);
    				data[addOffset] ^= (Uint8)corrValue;
    				// Fall through to case 1
    			case 1:     // Two errors
    				addOffset = 519 - ( (AEMIF->NANDERRADD1 & (0x03FF0000))>>16 );
    				if (addOffset > 511) return E_FAIL;
    				corrValue = (AEMIF->NANDERRVAL1 & (0x03FF0000))>>16;
    				data[addOffset] ^= (Uint8)corrValue;
    				// Fall through to case 0
    			case 0:     // One error
    				addOffset = 519 - (AEMIF->NANDERRADD1 & (0x000003FF));
    				if (addOffset > 511) return E_FAIL;
    				corrValue = AEMIF->NANDERRVAL1 & (0x3FF);
    				data[addOffset] ^= (Uint8)corrValue;
    				break;
    		}
    		return E_PASS;
    	}
    }
    
    // Function to manipulate the spare bytes to mark as a bad block
    static void DEVICE_NAND_BB_markSpareBytes(NAND_InfoHandle hNandInfo, Uint8 *spareBytes)
    {
    	Uint32		i, j;
    	// Mark all the free bytes (non-ECC bytes) as 0x00
    	for (j = 0; j< hNandInfo->numOpsPerPage; j++){
    		for (i=0; i<DEVICE_NAND_ECC_START_OFFSET; i++){
    			spareBytes[i+hNandInfo->spareBytesPerOp*j] = 0x00;
    		}
    	}
    }
    
    // Function to determine if the spare bytes indicate a bad block
    static Uint32 DEVICE_NAND_BB_checkSpareBytes(NAND_InfoHandle hNandInfo, Uint8 *spareBytes)
    {
    	Uint32		i, j;
    	// Check all the free bytes (non-ECC bytes) for 0xFF
    	for (j = 0; j< hNandInfo->numOpsPerPage; j++){
    		for (i=0; i<DEVICE_NAND_ECC_START_OFFSET; i++){
    			if (spareBytes[i+hNandInfo->spareBytesPerOp*j] != 0xFF)
    				return E_FAIL;
    		}
    	}
    
    	return E_PASS;
    }
    
    /***********************************************************
    * End file                                                 *
    ***********************************************************/
    
    
    

  • Basically the ECC is calculated for all the data that is transferred through the data bus, once the ECC engine is turned on. So, to understand the calculation, we need to understand exactly how many bytes transfer is happening in the bus.

    Can you attach the file where these functions are called? The function pointers will be used there. 


  • Hello, Renjith-san.

    I am facing same phenomenon.
    I have refered the EMIF UG(sprufi1c: P28).

    Since the EMIF is supported 4bit ECC calculation up to 518 byte, addOffset maximum value can be 517.
    addOffset is parameter in the DEVICE_NAND_ECC_correct() device_nand.c.
    I think the below souce code should be evaluate whether its value is more than 518.
    How do you think about this?

    Yoichi said:

    device_nand.c line 287:

      switch( numE ){
       case 3:     // Four errors
        addOffset = 519 - ( (AEMIF->NANDERRADD2 & (0x03FF0000))>>16 );
        if (addOffset > 511) return E_FAIL;
        corrValue = (AEMIF->NANDERRVAL2 & (0x03FF0000))>>16;
        data[addOffset] ^= (Uint8)corrValue;
        // Fall through to case 2
       case 2:     // Three errors
        addOffset = 519 - (AEMIF->NANDERRADD2 & (0x000003FF));
        if (addOffset > 511) return E_FAIL;
        corrValue = AEMIF->NANDERRVAL2 & (0x000003FF);
        data[addOffset] ^= (Uint8)corrValue;
        // Fall through to case 1
       case 1:     // Two errors
        addOffset = 519 - ( (AEMIF->NANDERRADD1 & (0x03FF0000))>>16 );
        if (addOffset > 511) return E_FAIL;
        corrValue = (AEMIF->NANDERRVAL1 & (0x03FF0000))>>16;
        data[addOffset] ^= (Uint8)corrValue;
        // Fall through to case 0
       case 0:     // One error
        addOffset = 519 - (AEMIF->NANDERRADD1 & (0x000003FF));
        if (addOffset > 511) return E_FAIL;
        corrValue = AEMIF->NANDERRVAL1 & (0x3FF);
        data[addOffset] ^= (Uint8)corrValue;
        break;
      }

     

  • RY,

    There is something wrong in using 519 itself. I believe this needs more debugging. 

  • Renjith-san,
    Thank you so much for your advise.
    I would like to check the Reed solomon ecc algorithm which is used in DM365 EMIF.
    If I found something, I will get back to you.
    Best regards, RY


  • Renjith-san,
    Hello, I am checking ECC.
    There is description about 4-bit Reed Solomon ECC in the following URL.
    http://processors.wiki.ti.com/index.php/NAND_ECC_Generation_for_DaVinci_Family_of_Devices#GenECC_Applications

    It describes that:
      Note that in the case of the Reed Solomon ECC, each register actually contains
      only 20 bits of ECC parity information, for a total of 80 bits.
      How those bits of information should be stored in the spare bytes of the NAND device,
      such that the ROM boot loader can correctly interpret them during read back at boot time,
      may be device dependent. Please consult with the device's datasheet and system guides
      for details.

    I would like to know about DM365 RBL ECC.
    Where can I get the 20 bits of ECC parity information?

    Best regards, RY