Dears,
we now use TVSVC5502 in our product, using CCS4.2 in WINXP SP3, as debug using JTAG(small test code,runs OK in .cmd and .gel ), can download and debug, but also followed by:
=========================================================================
Occured at 0x0000101A
C55xx: Trouble Reading Memory Block at 0x80e on Page 2 of Length 0x1: Error 0x00000002/-1069 Error during: Memory, PTI_ERR_MEM_BUSERR Error Occured at 0x0000101C
C55xx: Trouble Reading Memory Block at 0x80f on Page 2 of Length 0x1: Error 0x00000002/-1069 Error during: Memory, PTI_ERR_MEM_BUSERR Error Occured at 0x0000101E ==========================================================================
it seems few rams are bad,but not all. we changes 4 boards, same errors coming.
now our proj is tight,so we urgently want to now the reason and the resolve method.
thanks.