This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Booting fails with BBB

Other Parts Discussed in Thread: TPS65910, TPS65217, DA8XX

Hello All,
I am using beagleboneblack with Android JB for my development,I have configured to my u-boot in u-boot/board/ti/am335x/board.c .But it is not getting booted. Is there any solution to boot with the above mentioned configuration by skipping from eeprom.

                                                              Thanks in advance.

  • Hi.

    Which part of code are you modifying.

    You need not modify/configure u-boot for Beaglebone black. Existing u-boot should work straight a way.

    Please try booting with the Prebuilt image available on below release page (Under "Pre-built Images" section).

    http://downloads.ti.com/sitara_android/esd/TI_Android_DevKit/TI_Android_JB_4_2_2_DevKit_4_1_1/index_FDS.html

    Regards,

    Pankaj Bharadiya

  • Hello Pankaj,

                           Thanks for your reply.Sorry for above mentioned post,I have missed with some data's. The thing is,

    I  need to boot BBB using eMMC  with Android JB 4.2.2(latest version) ,for me the booting fails .  And i follow 

    http://processors.wiki.ti.com/index.php/TI-Android-JB-4.2.2-DevKit-4.1.1_DeveloperGuide#Fastboot_and_eMMC

    to boot using emmc.

                                                    Thanks in advance.

  • Hi,

    What  kind of issues are you facing?

    Will you please elaborate.

    Regards,

    Pankaj Bharadiya

  • Hi,
         Sorry for the delay in reponse i was trying with Android 4.1.2 . Now , I am using BBB with Android 4.1.2 for booting with eMMC.

    For that i follow the below link
    http://processors.wiki.ti.com/index.php/TI-Android-JB-4.2.2-DevKit-4.1.1_DeveloperGuide#Fastboot_and_eMMC

    But the booting is not successful.

    The logcat for booting with eMMC are as follows,

    downloading of 201326592 bytes finished
    .mmc1(part 0) is current device
    Initializing 'cache'
    mmc_send_cmd : timeout: No status update
    Writing 'cache'

    MMC write: dev # 1, block # 559104, count 393217 ... 393217 blocks write: OK
    Writing 'cache' DONE!
    resetting ...

    U-Boot SPL 2013.01.01 (Sep 19 2013 - 13:13:19)
    musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
    musb-hdrc: MHDRC RTL version 2.0
    musb-hdrc: setup fifo_mode 4
    musb-hdrc: 28/31 max ep, 16384/16384 memory
    USB Peripheral mode controller at 47401000 using PIO, IRQ 0
    musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
    musb-hdrc: MHDRC RTL version 2.0
    musb-hdrc: setup fifo_mode 4
    musb-hdrc: 28/31 max ep, 16384/16384 memory
    USB Host mode controller at 47401800 using PIO, IRQ 0
    OMAP SD/MMC: 0
    reading u-boot.img
    reading u-boot.img


    U-Boot 2013.01.01 (Sep 19 2013 - 13:13:19)

    I2C: ready
    DRAM: 512 MiB
    WARNING: Caches not enabled
    NAND: No NAND device found!!!
    0 MiB
    MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
    *** Warning - readenv() failed, using default environment

    musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
    musb-hdrc: MHDRC RTL version 2.0
    musb-hdrc: setup fifo_mode 4
    musb-hdrc: 28/31 max ep, 16384/16384 memory
    USB Peripheral mode controller at 47401000 using PIO, IRQ 0
    musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
    musb-hdrc: MHDRC RTL version 2.0
    musb-hdrc: setup fifo_mode 4
    musb-hdrc: 28/31 max ep, 16384/16384 memory
    USB Host mode controller at 47401800 using PIO, IRQ 0
    Net: <ethaddr> not set. Validating first E-fuse MAC
    cpsw
    Hit any key to stop autoboot: 0
    mmc_send_cmd : timeout: No status update
    mmc1(part 0) is current device
    mmc_send_cmd : timeout: No status update
    Loading efi partition table:

    MMC read: dev # 1, block # 1, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 1, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 2, count 1 ... 1 blocks read: OK
    256 128K spl
    512 512K bootloader
    1536 128K misc
    2048 8M recovery

    MMC read: dev # 1, block # 3, count 1 ... 1 blocks read: OK
    18432 8M boot
    34816 256M system
    559104 256M cache
    1083392 256M userdata

    MMC read: dev # 1, block # 4, count 1 ... 1 blocks read: OK
    1607680 1047M media

    MMC read: dev # 1, block # 5, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 6, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 7, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 8, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 9, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 10, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 11, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 12, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 13, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 14, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 15, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 16, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 17, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 18, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 19, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 20, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 21, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 22, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 23, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 24, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 25, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 26, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 27, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 28, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 29, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 30, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 31, count 1 ... 1 blocks read: OK

    MMC read: dev # 1, block # 32, count 1 ... 1 blocks read: OK
    Loaded eMMC partition table
    SELECT MMC DEV: 1
    mmc1(part 0) is current device
    mmc_send_cmd : timeout: No status update

    MMC read: dev # 1, block # 18432, count 1 ... 1 blocks read: OK
    Image magic: ANDROID!Xc@
    kernel_size: 0x406358
    kernel_addr: 0x80008000
    rdisk_size: 0x28cb6
    rdisk_addr: 0x81000000
    second_size: 0x0
    second_addr: 0x80f00000
    tags_addr: 0x80000100
    page_size: 0x800
    name:
    cmdline: 0x9fb96e80
    id[0]: 0x0
    id[1]: 0x0
    id[2]: 0x0
    id[3]: 0x0
    id[4]: 0x0
    id[5]: 0x0
    id[6]: 0x0
    id[7]: 0x0

    Header: Kernel Addr:0x80008000
    Header: Kernel Size:0x406358
    Header: Ramdisk Addr:0x81000000
    Header: Ramdisk Size:0x28cb6

    ramdisk sector count:326
    MMC read: dev # 1, block # 18436, count 8242 ... 8242 blocks read: OK


    ramdisk sector count:326
    MMC read: dev # 1, block # 26680, count 327 ... 327 blocks read: OK
    kernel @ 80008000 (4219736)
    ramdisk @ 81000000 (167094)

    Starting kernel ...


    Cleanup before kernel ...


    Starting kernel, theKernel ...

    Uncompressing Linux... done, booting the kernel.
    [ 0.000000] Linux version 3.2.0 (marudham@marudham-desktop) (gcc version 4.4.3 (GCC) ) #1 Thu Sep 19 00:08:29 IST 2013
    [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
    [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
    [ 0.000000] Machine: am335xevm
    [ 0.000000] Memory policy: ECC disabled, Data cache writeback
    [ 0.000000] AM335X ES2.0 (sgx neon )
    [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048
    [ 0.000000] Kernel command line: console=ttyO0,115200n8 androidboot.console=ttyO0 mem=512M root=/dev/ram0 rw initramfs=0x81000000,8M init=/init ip=off
    [ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
    [ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
    [ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
    [ 0.000000] Memory: 512MB = 512MB total
    [ 0.000000] Memory: 509628k/509628k available, 14660k reserved, 0K highmem
    [ 0.000000] Virtual kernel memory layout:
    [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
    [ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
    [ 0.000000] vmalloc : 0xe0800000 - 0xff000000 ( 488 MB)
    [ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
    [ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
    [ 0.000000] .text : 0xc0008000 - 0xc07a0000 (7776 kB)
    [ 0.000000] .init : 0xc07a0000 - 0xc07f6000 ( 344 kB)
    [ 0.000000] .data : 0xc07f6000 - 0xc08617f0 ( 430 kB)
    [ 0.000000] .bss : 0xc0861814 - 0xc09b9498 (1376 kB)
    [ 0.000000] NR_IRQS:396
    [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
    [ 0.000000] Total of 128 interrupts on 1 active controller
    [ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
    [ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
    [ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
    [ 0.000000] Console: colour dummy device 80x30
    [ 0.000091] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736)
    [ 0.088836] pid_max: default: 32768 minimum: 301
    [ 0.088958] Security Framework initialized
    [ 0.089019] Mount-cache hash table entries: 512
    [ 0.089355] CPU: Testing write buffer coherency: ok
    [ 0.089416] ftrace: allocating 22304 entries in 66 pages
    [ 0.145843] omap_hwmod: pruss: failed to hardreset
    [ 0.146514] print_constraints: dummy:
    [ 0.146697] NET: Registered protocol family 16
    [ 0.147583] OMAP GPIO hardware version 0.1
    [ 0.148437] omap_mux_init: Add partition: #1: core, flags: 0
    [ 0.149353] omap_i2c.1: alias fck already exists
    [ 0.149780] omap2_mcspi.1: alias fck already exists
    [ 0.149871] omap2_mcspi.2: alias fck already exists
    [ 0.149963] edma.0: alias fck already exists
    [ 0.149993] edma.0: alias fck already exists
    [ 0.149993] edma.0: alias fck already exists
    [ 0.157684] bio: create slab <bio-0> at 0
    [ 0.158477] SCSI subsystem initialized
    [ 0.159210] usbcore: registered new interface driver usbfs
    [ 0.159301] usbcore: registered new interface driver hub
    [ 0.159423] usbcore: registered new device driver usb
    [ 0.159667] registerd cppi-dma Intr @ IRQ 17
    [ 0.159667] Cppi41 Init Done Qmgr-base(e087a000) dma-base(e0878000)
    [ 0.159698] Cppi41 Init Done
    [ 0.159698] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3
    [ 0.159820] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1
    [ 0.160186] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
    [ 0.160827] tps65910 1-002d: could not be detected
    [ 0.161254] Advanced Linux Sound Architecture Driver Version 1.0.24.
    [ 0.161682] Bluetooth: Core ver 2.16
    [ 0.161743] NET: Registered protocol family 31
    [ 0.161743] Bluetooth: HCI device and connection manager initialized
    [ 0.161773] Bluetooth: HCI socket layer initialized
    [ 0.161773] Bluetooth: L2CAP socket layer initialized
    [ 0.161804] Bluetooth: SCO socket layer initialized
    [ 0.161956] Switching to clocksource gp timer
    [ 0.176544] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
    [ 0.176727] musb-hdrc musb-hdrc.0: dma type: dma-cppi41
    [ 0.176879] MUSB0 controller's USBSS revision = 4ea20800
    [ 0.176910] musb0: Enabled SW babble control
    [ 0.177612] musb-hdrc musb-hdrc.0: USB OTG mode controller at e083c000 using DMA, IRQ 18
    [ 0.177825] musb-hdrc musb-hdrc.1: dma type: dma-cppi41
    [ 0.177978] MUSB1 controller's USBSS revision = 4ea20800
    [ 0.178009] musb1: Enabled SW babble control
    [ 0.178314] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
    [ 0.178405] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
    [ 0.178527] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
    [ 0.178527] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [ 0.178558] usb usb1: Product: MUSB HDRC host driver
    [ 0.178558] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd
    [ 0.178558] usb usb1: SerialNumber: musb-hdrc.1
    [ 0.178955] hub 1-0:1.0: USB hub found
    [ 0.178985] hub 1-0:1.0: 1 port detected
    [ 0.179290] musb-hdrc musb-hdrc.1: USB Host mode controller at e083e800 using DMA, IRQ 19
    [ 0.179595] NET: Registered protocol family 2
    [ 0.179748] IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
    [ 0.180084] TCP established hash table entries: 16384 (order: 5, 131072 bytes)
    [ 0.180297] TCP bind hash table entries: 16384 (order: 4, 65536 bytes)
    [ 0.180419] TCP: Hash tables configured (established 16384 bind 16384)
    [ 0.180450] TCP reno registered
    [ 0.180450] UDP hash table entries: 256 (order: 0, 4096 bytes)
    [ 0.180480] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
    [ 0.180633] NET: Registered protocol family 1
    [ 0.180877] RPC: Registered named UNIX socket transport module.
    [ 0.180877] RPC: Registered udp transport module.
    [ 0.180908] RPC: Registered tcp transport module.
    [ 0.180908] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [ 0.181121] Trying to unpack rootfs image as initramfs...
    [ 0.191131] Freeing initrd memory: 160K
    [ 0.191131] NetWinder Floating Point Emulator V0.97 (double precision)
    [ 0.288116] ashmem: initialized
    [ 0.288360] VFS: Disk quotas dquot_6.5.2
    [ 0.288391] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
    [ 0.289093] fuse init (API version 7.17)
    [ 0.289306] msgmni has been set to 995
    [ 0.290100] io scheduler noop registered
    [ 0.290130] io scheduler deadline registered
    [ 0.290191] io scheduler cfq registered (default)
    [ 0.290649] Could not set LED4 to fully on
    [ 0.322662] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
    [ 0.948272] console [ttyO0] enabled
    [ 0.952239] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
    [ 0.959869] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
    [ 0.967468] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
    [ 0.975097] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
    [ 0.982696] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
    [ 0.990386] [drm] Initialized drm 1.1.0 20060810
    [ 0.999664] brd: module loaded
    [ 1.005340] loop: module loaded
    [ 1.008758] i2c-core: driver [tsl2550] using legacy suspend method
    [ 1.015258] i2c-core: driver [tsl2550] using legacy resume method
    [ 1.021667] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
    [ 1.122528] No daughter card found on AM335x EVM
    [ 1.127410] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
    [ 1.142608] Board name: A335BNLT
    [ 1.145965] Board version: 0A5B
    [ 1.149230] The board is a AM335x Beaglebone Black.
    [ 1.156127] tps65217 1-0024: TPS65217 ID 0xe version 1.2
    [ 1.163391] print_constraints: DCDC1: 900 <--> 1800 mV at 1500 mV
    [ 1.171569] print_constraints: DCDC2: 900 <--> 3300 mV at 1325 mV
    [ 1.179779] print_constraints: DCDC3: 900 <--> 1500 mV at 1125 mV
    [ 1.187957] print_constraints: LDO1: 1000 <--> 3300 mV at 1800 mV
    [ 1.196166] print_constraints: LDO2: 900 <--> 3300 mV at 3300 mV
    [ 1.204254] print_constraints: LDO3: 1800 <--> 3300 mV at 1800 mV
    [ 1.212432] print_constraints: LDO4: 1800 <--> 3300 mV at 3300 mV
    [ 1.222167] omap_hsmmc.0: alias fck already exists
    [ 1.227416] omap_hsmmc.1: alias fck already exists
    [ 1.232696] omap_i2c.3: alias fck already exists
    [ 1.237792] omap_i2c omap_i2c.3: bus 3 rev2.4.0 at 100 kHz
    [ 1.244873] at24 3-0054: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
    [ 1.252166] IN : bone_setup_display_daughter_board
    [ 1.352539] No display cape found on BeagleBone
    [ 1.357757] da8xx_lcdc.0: alias fck already exists
    [ 1.363037] da8xx_lcdc da8xx_lcdc.0: GLCD: Found nxp-1280x720@60 panel
    [ 1.514953] tda998x 1-0070: found TDA19988
    [ 3.542602] tda998x 1-0070: failed to read EDID
    [ 3.565063] Setup HDMI display complete
    [ 3.569122] at24 3-0055: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
    [ 3.576385] IN : bone_setup_daughter_board
    [ 3.672607] at24 3-0056: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
    [ 3.679901] IN : bone_setup_daughter_board
    [ 3.762634] at24 3-0057: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
    [ 3.769897] IN : bone_setup_daughter_board
    [ 3.872741] (hci_tty): inside hci_tty_init
    [ 3.877166] (hci_tty): allocated 251, 0
    [ 3.881286] NFC Driver for TI WiLink
    [ 3.885559] mtdoops: mtd device (mtddev=name/number) must be supplied
    [ 3.892639] omap2-nand driver initializing
    [ 3.896972] OneNAND driver initializing
    [ 3.901367] CAN device driver interface
    [ 3.905395] CAN bus driver for Bosch D_CAN controller 1.0
    [ 3.952606] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
    [ 3.959075] davinci_mdio davinci_mdio.0: detected phy mask fffffffe
    [ 3.966400] davinci_mdio.0: probed
    [ 3.969970] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver SMSC LAN8710/LAN8720
    [ 3.978607] PPP generic driver version 2.4.2
    [ 3.983215] PPP BSD Compression module registered
    [ 3.988128] PPP Deflate Compression module registered
    [ 3.993530] usbcore: registered new interface driver cdc_ether
    [ 3.999664] usbcore: registered new interface driver cdc_eem
    [ 4.005645] usbcore: registered new interface driver dm9601
    [ 4.011505] usbcore: registered new interface driver cdc_subset
    [ 4.017730] cdc_ncm: 04-Aug-2011
    [ 4.021148] usbcore: registered new interface driver cdc_ncm
    [ 4.027130] usbcore: registered new interface driver cdc_acm
    [ 4.033050] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
    [ 4.041442] Initializing USB Mass Storage driver...
    [ 4.046630] usbcore: registered new interface driver usb-storage
    [ 4.052917] USB Mass Storage support registered.
    [ 4.057891] usbcore: registered new interface driver usbserial
    [ 4.064025] USB Serial support registered for generic
    [ 4.069366] usbcore: registered new interface driver usbserial_generic
    [ 4.076202] usbserial: USB Serial Driver core
    [ 4.080780] USB Serial support registered for GSM modem (1-port)
    [ 4.087158] usbcore: registered new interface driver option
    [ 4.093017] option: v0.7.2:USB Driver for GSM modems
    [ 4.099487] gadget: Mass Storage Function, version: 2009/09/11
    [ 4.105712] gadget: Number of LUNs=1
    [ 4.109558] lun0: LUN: removable file: (no medium)
    [ 4.114837] gadget: android_usb ready
    [ 4.118774] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
    [ 4.124389] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2
    [ 4.132232] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
    [ 4.139343] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [ 4.146911] usb usb2: Product: MUSB HDRC host driver
    [ 4.152069] usb usb2: Manufacturer: Linux 3.2.0 musb-hcd
    [ 4.157653] usb usb2: SerialNumber: musb-hdrc.0
    [ 4.162780] hub 2-0:1.0: USB hub found
    [ 4.166687] hub 2-0:1.0: 1 port detected
    [ 4.171325] mousedev: PS/2 mouse device common for all mice
    [ 4.178100] using rtc device, am33xx-rtc, for alarms
    [ 4.183197] omap_rtc am33xx-rtc: rtc core: registered am33xx-rtc as rtc0
    [ 4.190399] am33xx-rtc: already running
    [ 4.194488] i2c /dev entries driver
    [ 4.198394] Linux video capture interface: v2.00
    [ 4.203491] usbcore: registered new interface driver uvcvideo
    [ 4.209503] USB Video Class driver (1.1.1)
    [ 4.453247] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
    [ 4.459747] device-mapper: uevent: version 1.0.3
    [ 4.464752] device-mapper: ioctl: 4.22.0-ioctl (2011-10-19) initialised: dm-devel@redhat.com
    [ 4.473602] Bluetooth: HCI UART driver ver 2.2
    [ 4.478240] Bluetooth: HCI H4 protocol initialized
    [ 4.483245] Bluetooth: HCILL protocol initialized
    [ 4.488159] Bluetooth: Bluetooth Driver for TI WiLink - Version 1.0
    [ 4.570281] cpuidle: using governor ladder
    [ 4.574737] cpuidle: using governor menu
    [ 4.582336] usbcore: registered new interface driver usbhid
    [ 4.588226] usbhid: USB HID core driver
    [ 4.592651] logger: created 256K log 'log_main'
    [ 4.597503] logger: created 256K log 'log_events'
    [ 4.602539] logger: created 256K log 'log_radio'
    [ 4.607482] logger: created 256K log 'log_system'
    [ 4.612945] usbcore: registered new interface driver snd-usb-audio
    [ 4.620239] ALSA device list:
    [ 4.623382] No soundcards found.
    [ 4.626922] oprofile: hardware counters not available
    [ 4.632202] oprofile: using timer interrupt.
    [ 4.636840] Netfilter messages via NETLINK v0.30.
    [ 4.641906] nf_conntrack version 0.5.0 (7965 buckets, 31860 max)
    [ 4.648529] ctnetlink v0.93: registering with nfnetlink.
    [ 4.654174] NF_TPROXY: Transparent proxy support initialized, version 4.1.0
    [ 4.661468] NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.
    [ 4.667907] xt_time: kernel timezone is -0000
    [ 4.672698] ip_tables: (C) 2000-2006 Netfilter Core Team
    [ 4.678466] arp_tables: (C) 2002 David S. Miller
    [ 4.683410] TCP cubic registered
    [ 4.686920] NET: Registered protocol family 10
    [ 4.692321] Mobile IPv6
    [ 4.694946] ip6_tables: (C) 2000-2006 Netfilter Core Team
    [ 4.700775] IPv6 over IPv4 tunneling driver
    [ 4.705749] NET: Registered protocol family 17
    [ 4.710449] NET: Registered protocol family 15
    [ 4.715118] can: controller area network core (rev 20090105 abi 8)
    [ 4.721710] NET: Registered protocol family 29
    [ 4.726379] can: raw protocol (rev 20090105)
    [ 4.730865] can: broadcast manager protocol (rev 20090105 t)
    [ 4.737213] Bluetooth: RFCOMM TTY layer initialized
    [ 4.742340] Bluetooth: RFCOMM socket layer initialized
    [ 4.747741] Bluetooth: RFCOMM ver 1.11
    [ 4.751647] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
    [ 4.757232] Bluetooth: BNEP filters: protocol multicast
    [ 4.762695] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
    [ 4.769042] Registering the dns_resolver key type
    [ 4.774047] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
    [ 4.782073] ThumbEE CPU extension supported.
    [ 4.786621] mux: Failed to setup hwmod io irq -22
    [ 4.792236] Power Management for AM33XX family
    [ 4.797119] Trying to load am335x-pm-firmware.bin (60 secs timeout)
    [ 4.803802] Copied the M3 firmware to UMEM
    [ 4.808166] Cortex M3 Firmware Version = 0x181
    [ 4.816406] clock: disabling unused clocks to save power
    [ 4.823364] Detected MACID=c8:a0:30:a8:a:82
    [ 4.828918] omap_rtc am33xx-rtc: setting system clock to 2000-01-01 00:41:38 UTC (946687298)
    [ 4.838653] Freeing init memory: 344K
    [ 4.853546] init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead.
    [ 4.890197] mmc0: host does not support reading read-only switch. assuming write-enable.
    [ 4.909240] mmc0: new high speed SD card at address b368
    [ 4.919342] mmcblk0: mmc0:b368 00000 1.83 GiB
    [ 4.929473] mmcblk0: p1 p2 p3 p4
    [ 4.950103] init: cannot open '/initlogo.rle'
    [ 4.963317] init: cannot find '/system/bin/servicemanager', disabling 'servicemanager'
    [ 4.971649] init: cannot find '/system/bin/vold', disabling 'vold'
    [ 4.978210] init: cannot find '/system/bin/sgx/rc.pvr', disabling 'pvr'
    [ 4.985260] init: cannot find '/system/bin/uim-sysfs', disabling 'uim'
    [ 4.993194] init: cannot find '/system/bin/netd', disabling 'netd'
    [ 5.001708] init: cannot find '/system/bin/debuggerd', disabling 'debuggerd'
    [ 5.009155] init: cannot find '/system/bin/rild', disabling 'ril-daemon'
    [ 5.016265] init: cannot find '/system/bin/surfaceflinger', disabling 'surfaceflinger'
    [ 5.024597] init: cannot find '/system/bin/app_process', disabling 'zygote'
    [ 5.031951] init: cannot find '/system/bin/drmserver', disabling 'drm'
    [ 5.038940] init: cannot find '/system/bin/mediaserver', disabling 'media'
    [ 5.046234] init: cannot find '/system/bin/dbus-daemon', disabling 'dbus'
    [ 5.053405] init: cannot find '/system/bin/installd', disabling 'installd'
    [ 5.060668] init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
    [ 5.069671] init: cannot find '/system/bin/keystore', disabling 'keystore'
    [ 5.080352] init: property 'ro.product.manufacturer' doesn't exist while expanding '${ro.product.manufacturer}'
    [ 5.091003] init: cannot expand '${ro.product.manufacturer}' while writing to '/sys/class/android_usb/android0/iManufacturer'
    [ 5.102874] init: property 'ro.product.model' doesn't exist while expanding '${ro.product.model}'
    [ 5.112182] init: cannot expand '${ro.product.model}' while writing to '/sys/class/android_usb/android0/iProduct'
    [ 5.123748] init: cannot find '/system/bin/sh', disabling 'console'
    [ 5.130493] android_usb: already disabled
    [ 5.135040] adb_bind_config
    [ 5.138275] adb_bind_config
    [ 5.143554] adb_open
    [ 5.148956] mmc1: new high speed MMC card at address 0001
    [ 5.155242] mmcblk1: mmc1:0001 MMC02G 1.78 GiB
    [ 5.160125] mmcblk1boot0: mmc1:0001 MMC02G partition 1 1.00 MiB
    [ 5.166473] mmcblk1boot1: mmc1:0001 MMC02G partition 2 1.00 MiB
    [ 5.178771] Alternate GPT is invalid, using primary GPT.
    [ 5.184509] mmcblk1: p1 p2 p3 p4 p5 p6 p7 p8 p9
    [ 5.194458] mmcblk1boot1: unknown partition table
    [ 5.201385] mmcblk1boot0: unknown partition table
    [ 5.464233] android_work: sent uevent USB_STATE=CONNECTED
    [ 5.469909] android_work: sent uevent USB_STATE=DISCONNECTED
    [ 5.614166] android_work: sent uevent USB_STATE=CONNECTED
    [ 5.620727] gadget: high-speed config #1: android
    [ 5.625823] android_work: sent uevent USB_STATE=CONFIGURED

    The changes where i made is that,
    In init.rc file i made some changes are as follows,

    on fs
    mount ext4 /dev/block/mmcblk1p6 /system wait ro
    mount ext4 /dev/block/mmcblk1p8 /data wait noatime nosuid nodev
    mount ext4 /dev/block/mmcblk1p7 /cache wait noatime nosuid nodev

    Faster reply will help me out for the better result.

    Thanks in advance.