Other Parts Discussed in Thread: AM3352, TPS65217
Hi all,
i'm quite new within the "Sitara" business and have a problem on a custom Board to drive a GPIO-Pin.
We're using the Sitara AM3352 processor.
The Application only does setup GPIO2_4 Pin and afterwards it wants to toggle the pin.
Power Rail VDDSHV is connectet to 3.3V
I can see toggling as expectet on the scope but drive strength is much too low. Output only reaches about 2.4V and connecting a few megaohms to ground lets drop the output downto about 1.5V.
Same application on the beagleboard is working.
We've allready checked voltages and powersequencing without success.
Any idea whats going wrong here ?