Other Parts Discussed in Thread: AM3352
Hello, Guru.
I have am3352 based board with with DDR2 chip MT47H32M16HR-25E. Oscillator clock frequency 25 Mhz. The board is now booting from mmc0.
In my code I 'm skipping i2c eeprom check, and execute some basic pin mux. Before loading image I performed memory tests with 0xAA 0x55 0x00 0xFF values.
U-Boot SPL 2013.01.01 (Sep 16 2013 - 13:58:48)
Memory Test!0x55 test passed0xAA test passed0x00 test passed0xFF test passedmusb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
OMAP SD/MMC: 0
reading u-boot.img
Then the device hangs. Could You please give me advice how to solve it? Thanks!