Hello,
We are using AM3730.
We’ve a battery charger(LTC4100) which communicates over SMBUS(I2C3 port).
As per SMBUS spec 1.1, Slave can hold the clock low till it is ready to respond.
Is I2C clock stretching is supported in AM3730? If Yes, How?, Do we need to do specific configurations in I2C for that?
Does AM3730 wince/linux driver supports smbus commands?
When AM3730 tries to communicate LTC4100 charger i.e. 0x9. It seems, it tries to ACK, however, At the 9th clock data and clock is not proper. Please find the waveform as below.