This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SMBUS on AM3730 Wince 6.0

Hello,

We are using AM3730 with wince 6.0.

We’ve a battery charger(LTC4100) which communicates over SMBUS(I2C3 port). 

As per SMBUS spec 1.1, Slave can hold the clock low till it is ready to respond.

Is I2C clock stretching is supported in AM3730? If Yes, How?, Do we need to do specific configurations in I2C for that?

Does AM3730 wince I2C driver supports smbus commands? Do you have sample driver for AM3730?