This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Clear GPIO IRQ status before enable in linux



It seems I am getting a 'ghost' interrupt from my gpio.  I suspect that the IRQ status bits are set when I enable the interrupt and cause the interrupt to trigger even without changing the state on the gpio pin.  I am trying to find a kernel API  like _clear_gpio_irqstatus from drivers/gpio/gpio-omap.c.  To prevent the 'ghost' interrupt from occurring, the steps would be:

_clear_gpio_irqstatus()  // clear old interrupts from before

enable_irq() // enable the gpio interrupt

If someone can suggest something like _clear_gpio_irqstatus() that I can call from my driver, I'd appreciate it.  Or, if none exists, if there are hooks to access the gpio control registers.  I'm developing on an AM335x GP EVM with SDK 05.07.00.00.