This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6657 pads diameter

Hi,

From the C6657 data sheet, I am not sure which is the pads diameter, would u pls help provide the pads diameter?

Thanks very much and BR,

Andy

  • Hi Andy,

    Section 9.1 of the Hardware Design Guide for KeyStone Devices discusses the layout guidelines for the BGA. If refers to SPRU811 Flip Chip Ball Grid Array Package Reference Guide which contains land and solder mask information in section 3.2.1. Table 2 in that section specifies the PCB copper land for parts with a ball pitch of 0.8mm as 0.45mm or approximately 18mil. Section 3.2.1 contains details on the reason that this is the best pad size to use.

    Regards, Bill