Hi,
I need to test JPEG2000 decoding on Shannon and judging by the "JPEG2K DECODER (v01.00.00.00) on C66x datasheet" in "J2D_DEC_L5" configuration, it would require around 2-3 Shannon chips.
Would it be possible to effectively compose two or three Shannon based device by separately connecting two or three TMDSEVM6678LX evaluation modules to PCI-e through TMDXEVMPCI AMC to PCI adapter cards.
If so what are the modifications needed to MCSDK to test JPEG2000 decoder. DSPC 8681 is steeper in price still for dual Shannon requirement hence posting this.
Please help.