My question is that the Keystone hardware design guide has minimum decoupling requirements for all the rails but the eval card does not follow this and has much less than the guide advises, why? The guide advises to use 470uF caps with max ESR of 12mOhm and we are not sure these exist. This is for the
TI TMDSEVM6657LS
Also, When using a single DDR3 device with the C6657, is end termination advised for the address and control lines?
Please advise.
Thanks!!