This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Floating point limitation for C6747

Hi ,

I am using C6747 on OMAP137. I had ran my algorithm realtime mode using double precision successfully, but  I just change double to float variable, it has problem.  I have some question about this issue

1. What is floating point limitation for C6747?   

2. Could you reply maximum number and minim number for float variable?

 for example, -1.0 x 10^-??  ~ 1.0 x 10^??

Thank you

Doug 

  • Hi Doug,

    Thanks for your post.

    There are standard single and double precision formats mentioned in the C674x DSP CPU and Instruction Set, in which please refer Section 3.3.1 & 3.3.2 as below:

    http://www.ti.com/lit/ug/sprufe8b/sprufe8b.pdf

    Thanks & regards,

    Sivaraj K

    -------------------------------------------------------------------------------------------------------
    Please click the Verify Answer button on this post if it answers your question.
    --------------------------------------------------------------------------------------------------------
  • Hi Doug,

    In the most common format (ANSI/IEEE Std. 754-1985), the largest and smallest numbers are ±3.4×1038 and 1.2x10-38, respectively.

    Thanks & regards,

    Sivaraj K

    -------------------------------------------------------------------------------------------------------
    Please click the Verify Answer button on this post if it answers your question.
    --------------------------------------------------------------------------------------------------------

  • I saw in the document,

    Normalized: -1s ×2(e - 127) ×1.f 0<e<255

    Denormalized (Subnormal): -1s × 2-126 × 0.f e = 0; f is nonzero 

    but, I cannot understand  these number 3.4x10^38 and 1.2x10-38 ?


    Doug