Hi,
I'm new on NDK.
I just got c6678evm and I'm trying NDK helloworld example, but it does not work.
- CCSv5.3
- mcsdk_2_01_02_06 (patched)
- pre-build executable :<install_dir>\mcsdk_2_01_02_06\examples\ndk\helloWorld\evmc6678l\Debug\helloworld_evmc6678l.out
- NDK : ndk_2_21_01_38\packages\ti\ndk\winapps>helloWorld.exe
- Host OS : Windows7 64bit
- WinApp : <install_dir>\ndk_2_21_01_38\packages\ti\ndk\winapps>helloWorld.exe
Please note DIP switch has been configured not to work with DHCP on EVM.
QMSS successfully initialized
CPPI successfully initialized
PA successfully initialized
TCP/IP Stack 'Hello World!' Application
TCP/IP Stack 'Hello World!' Application
PASS successfully initialized
Ethernet subsystem successfully initialized
Ethernet eventId : 48 and vectId (Interrupt) : 7
Registration of the EMAC Successful, waiting for link up ..
Network Added: If-1:192.168.2.100
Kawada