This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Setting GPIO value

Hai

I'm Sekra working on beagleboard xm.Now i download the ICS source code for that board.It has 2.6.37 kernel (initial stable kernel) and u-boot 2010-dirty also.

In my u-boot i want to set the GPIO via the gpio.h functions respectively.

omap_request_gpio()

omap_set_gpio_direction()

 omap_get_gpio_datain() in the beagle.c file u-boot.

I want to configure with below commands instead of above ones 

gpio_request(N, "");

gpio_direction_output(N, 1);

gpio_set_value(N,0);

How do i change this functions....how do i cal this???what are the dependency files.

2)if i use to set the GPIO via the older functions ( omap_request_gpio ).How to set,clear,direction the pins??How to configure the GPIO via this commands respectively.