Other Parts Discussed in Thread: PMP, TVP5150, TVP7002
I am working on dm8168 processor, with ti-ezsdk_dm816x-evm_5_05_02_00 package and linux-2.6.37-psp04.04.00.01.
Now i am pursuing the camera testing. But i am getting a error
ti81xxvin ti81xxvin: Error registering v4l2 subdevice
like this when i try to insert ti81xxvin.
These are my boot log and commands i gave in console...
U-Boot 2010.06-svn220 (Sep 16 2013 - 12:32:05)
DRAM: 1 GiB
Using default environment
Hit any key to stop autoboot: 0
mmc1 is available
reading u-boot.bin
176048 bytes read
## Starting application at 0x80800000 ...
U-Boot 2010.06-svn220 (Sep 16 2013 - 12:34:09)
TI8168-GP rev 2.0
ARM clk: 987MHz
DDR clk: 796MHz
I2C: ready
DRAM: 1 GiB
NAND: HW ECC BCH8 Selected
128 MiB
*** Warning - bad CRC or NAND, using default environment
Hit any key to stop autoboot: 3 2 1 0
mmc1 is available
reading boot.scr
300 bytes read
Running bootscript from MMC/SD to set the ENV...
## Executing script at 80900000
reading uImage
2570792 bytes read
## Booting kernel from Legacy Image at 80009000 ...
Image Name: Linux-2.6.37
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2570728 Bytes = 2.5 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Linux version 2.6.37 (root@ajnac-OptiPlex-330) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #60 Wed Sep 18 12:01:42 IST 2013
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: ti8168evm
vram size = 52428800 at 0x0
reserved size = 52428800 at 0x0
FB: Reserving 52428800 bytes SDRAM for VRAM
Memory policy: ECC disabled, Data cache writeback
OMAP chip is TI8168 2.0
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 52224
Kernel command line: console=ttyO2,115200n8 rootwait root=/dev/mmcblk0p2 rw mem=256M earlyprink vram=50M ti816xfb.vram=0:16M,1:16M,2:6M ip=off noinitrd notifyk.vpssm3_sva=0xA0000000
PID hash table entries: 1024 (order: 0, 4096 bytes)
Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
Memory: 206MB = 206MB total
Memory: 203156k/203156k available, 58988k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
vmalloc : 0xd0800000 - 0xf8000000 ( 632 MB)
lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.init : 0xc0008000 - 0xc003c000 ( 208 kB)
.text : 0xc003c000 - 0xc04dc000 (4736 kB)
.data : 0xc04dc000 - 0xc0525300 ( 293 kB)
SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:407
IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
Total of 128 interrupts on 1 active controller
GPMC revision 6.0
Trying to install interrupt handler for IRQ400
Trying to install interrupt handler for IRQ401
Trying to install interrupt handler for IRQ402
Trying to install interrupt handler for IRQ403
Trying to install interrupt handler for IRQ404
Trying to install interrupt handler for IRQ405
Trying to install interrupt handler for IRQ406
Trying to install type control for IRQ407
Trying to set irq flags for IRQ407
OMAP clockevent source: GPTIMER1 at 27000000 Hz
Console: colour dummy device 80x30
Calibrating delay loop... 986.31 BogoMIPS (lpj=4931584)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
devtmpfs: initialized
omap_voltage_early_init: voltage driver support not added
regulator: core version 0.5
regulator: dummy:
NET: Registered protocol family 16
omap_voltage_domain_lookup: Voltage driver init not yet happened.Faulting!
omap_voltage_add_dev: VDD specified does not exist!
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
omap_mux_init: Add partition: #1: core, flags: 0
_omap_mux_get_by_name: Could not find signal i2c2_scl.i2c2_scl
_omap_mux_get_by_name: Could not find signal i2c2_sda.i2c2_sda
NOR: Can't request GPMC CS
registered ti816x_gpio_vr device
registered ti816x_sr device
pm_dbg_init: only OMAP3 supported
registered ti81xx_vpss device
registered ti81xx_vidout device
registered ti81xx on-chip HDMI device
registered ti81xx_fb device
registered ti81xx_vin device
ti81xx_pcie: Invoking PCI BIOS...
ti81xx_pcie: Setting up Host Controller...
ti81xx_pcie: Register base mapped @0xd0820000
ti81xx_pcie: Starting PCI scan...
PCI: bus0: Fast back to back transfers disabled
PCI: bus1: Fast back to back transfers disabled
PCI: bus2: Fast back to back transfers disabled
PCI: bus3: Fast back to back transfers enabled
PCI: bus4: Fast back to back transfers enabled
PCI: bus5: Fast back to back transfers disabled
pci 0000:00:00.0: BAR 8: assigned [mem 0x20000000-0x200fffff]
pci 0000:01:00.0: BAR 8: assigned [mem 0x20000000-0x200fffff]
pci 0000:02:03.0: BAR 8: assigned [mem 0x20000000-0x200fffff]
pci 0000:02:01.0: PCI bridge to [bus 03-03]
pci 0000:02:01.0: bridge window [io disabled]
pci 0000:02:01.0: bridge window [mem disabled]
pci 0000:02:01.0: bridge window [mem pref disabled]
pci 0000:02:02.0: PCI bridge to [bus 04-04]
pci 0000:02:02.0: bridge window [io disabled]
pci 0000:02:02.0: bridge window [mem disabled]
pci 0000:02:02.0: bridge window [mem pref disabled]
pci 0000:05:00.0: BAR 0: assigned [mem 0x20000000-0x2000ffff 64bit]
pci 0000:05:00.0: BAR 0: set to [mem 0x20000000-0x2000ffff 64bit] (PCI address [0x20000000-0x2000ffff])
pci 0000:05:00.0: BAR 2: assigned [mem 0x20010000-0x20011fff 64bit]
pci 0000:05:00.0: BAR 2: set to [mem 0x20010000-0x20011fff 64bit] (PCI address [0x20010000-0x20011fff])
pci 0000:02:03.0: PCI bridge to [bus 05-05]
pci 0000:02:03.0: bridge window [io disabled]
pci 0000:02:03.0: bridge window [mem 0x20000000-0x200fffff]
pci 0000:02:03.0: bridge window [mem pref disabled]
pci 0000:01:00.0: PCI bridge to [bus 02-05]
pci 0000:01:00.0: bridge window [io disabled]
pci 0000:01:00.0: bridge window [mem 0x20000000-0x200fffff]
pci 0000:01:00.0: bridge window [mem pref disabled]
pci 0000:00:00.0: PCI bridge to [bus 01-05]
pci 0000:00:00.0: bridge window [io disabled]
pci 0000:00:00.0: bridge window [mem 0x20000000-0x200fffff]
pci 0000:00:00.0: bridge window [mem pref disabled]
PCI: enabling device 0000:00:00.0 (0140 -> 0143)
PCI: enabling device 0000:01:00.0 (0140 -> 0143)
PCI: enabling device 0000:02:01.0 (0140 -> 0143)
PCI: enabling device 0000:02:02.0 (0140 -> 0143)
PCI: enabling device 0000:02:03.0 (0140 -> 0143)
bio: create slab <bio-0> at 0
regulator: VFB: 800 <--> 1025 mV at 1010 mV
vgaarb: loaded
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
USBSS revision 4ea20809
registerd cppi-dma Intr @ IRQ 17
Cppi41 Init Done
omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
omap_i2c omap_i2c.2: bus 2 rev4.0 at 100 kHz
Advanced Linux Sound Architecture Driver Version 1.0.23.
Switching to clocksource gp timer
musb-hdrc: version 6.0, host, debug=0
musb-hdrc musb-hdrc.0: dma type: dma-cppi41
MUSB controller-0 revision 4ea20800
musb-hdrc musb-hdrc.0: MUSB HDRC host driver
musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: MUSB HDRC host driver
usb usb1: Manufacturer: Linux 2.6.37 musb-hcd
usb usb1: SerialNumber: musb-hdrc.0
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
musb-hdrc musb-hdrc.0: USB Host mode controller at d081e000 using DMA, IRQ 18
musb-hdrc musb-hdrc.1: dma type: dma-cppi41
MUSB controller-1 revision 4ea20800
musb-hdrc musb-hdrc.1: MUSB HDRC host driver
musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: Product: MUSB HDRC host driver
usb usb2: Manufacturer: Linux 2.6.37 musb-hcd
usb usb2: SerialNumber: musb-hdrc.1
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
musb-hdrc musb-hdrc.1: USB Host mode controller at d0826800 using DMA, IRQ 19
NET: Registered protocol family 2
IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
TCP established hash table entries: 8192 (order: 4, 65536 bytes)
TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
NetWinder Floating Point Emulator V0.97 (double precision)
PMU: registered new PMU device of type 0
omap-iommu omap-iommu.0: ducati registered
omap-iommu omap-iommu.1: sys registered
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 396
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
console [ttyO2] enabled
brd: module loaded
loop: module loaded
ahci ahci.0: forcing PORTS_IMPL to 0x3
ahci ahci.0: AHCI 0001.0100 32 slots 2 ports 3 Gbps 0x3 impl platform mode
ahci ahci.0: flags: ncq sntf pm led clo only pmp pio slum part ccc
scsi0 : ahci_platform
scsi1 : ahci_platform
ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x100 irq 16
ata2: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x180 irq 16
omap2-nand driver initializing
NAND device: Manufacturer ID: 0xec, Chip ID: 0xf1 (Samsung )
Creating 5 MTD partitions on "omap2-nand.0":
0x000000000000-0x000000260000 : "U-Boot"
0x000000260000-0x000000280000 : "U-Boot Env"
0x000000280000-0x0000006c0000 : "Kernel"
0x0000006c0000-0x00000cee0000 : "File System"
mtd: partition "File System" extends beyond the end of device "omap2-nand.0" -- size truncated to 0x7940000
0x000008000000-0x000008000000 : "Reserved"
mtd: partition "Reserved" is out of reach -- disabled
davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
davinci_mdio davinci_mdio.0: detected phy mask fffffff7
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[3]: device 0:03, driver unknown
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver dm9601
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
mice: PS/2 mouse device common for all mice
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
i2c /dev entries driver
Linux video capture interface: v2.00
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v1.0.0)
OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
usb 1-1: new high speed USB device using musb-hdrc and address 2
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
notify_init : notify drivercreated for remote proc id 2 at physical Address 0xa0000000
usbcore: registered new interface driver snd-usb-audio
asoc: tlv320aic3x-hifi <-> davinci-mcasp.2 mapping ok
ALSA device list:
#0: TI81XX EVM
TCP cubic registered
NET: Registered protocol family 17
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
omap_voltage_late_init: Voltage driver support not added
Power Management for TI81XX.
smartreflex smartreflex: Driver initialized
DaVinci EMAC: No platform data
omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
ata2: SATA link down (SStatus 0 SControl 300)
mmc0: new high speed SDHC card at address aaaa
ata1: SATA link down (SStatus 0 SControl 300)
Waiting for root device /dev/mmcblk0p2...
mmcblk0: mmc0:aaaa SU04G 3.69 GiB
usb 1-1: New USB device found, idVendor=0424, idProduct=2514
usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
hub 1-1:1.0: USB hub found
mmcblk0: p1 p2
hub 1-1:1.0: 4 ports detected
EXT3-fs: barriers not enabled
kjournald starting. Commit interval 5 seconds
EXT3-fs (mmcblk0p2): warning: maximal mount count reached, running e2fsck is recommended
EXT3-fs (mmcblk0p2): using internal journal
EXT3-fs (mmcblk0p2): recovery complete
EXT3-fs (mmcblk0p2): mounted filesystem with writeback data mode
VFS: Mounted root (ext3 filesystem) on device 179:2.
devtmpfs: mounted
Freeing init memory: 208K
INIT: version 2.86 booting
Please wait: booting...
Error opening /dev/fb0: No such file or directory
Starting udev
udevd (72): /proc/72/oom_adj is deprecated, please use /proc/72/oom_score_adj instead.
Remounting root file system...
Caching udev devnodes
NET: Registered protocol family 10
ALSA: Restoring mixer settings...
Configuring network interfaces... No state is present for card EVM
Found hardware: "" "" "" "" ""
Hardware is initialized using a generic method
No state is present for card EVM
net eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:03, id=282f014)
ADDRCONF(NETDEV_UP): eth0: link is not ready
udhcpc (v1.13.2) started
Sending discover...
Sending discover...
Sending discover...
No lease, forking to background
done.
Setting up IP spoofing protection: rp_filter.
Wed Dec 26 15:58:00 UTC 2012
INIT: Entering runlevel: 5
Starting system message bus: dbus.
Starting telnet daemon.
Starting syslogd/klogd: done
Starting thttpd.
Starting Matrix GUI application.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org dm816x-evm ttyO2
Arago 2011.09 dm816x-evm ttyO2
dm816x-evm login: root
root@dm816x-evm:~# insmod /lib/modules/2.6.37/kernel/drivers/dsp/syslink.ko
SysLink version : 2.20.02.20
SysLink module created on Date:Dec 26 2012 Time:11:03:34
root@dm816x-evm:~# ./slaveloader startup VPSS-M3 ti816x_hdvpss.xem3
Attached to slave procId 2.
Loading procId 2.
Loaded file ti816x_hdvpss.xem3 on slave procId 2.
Started slave procId 2.
root@dm816x-evm:~# insmod /lib/modules/2.6.37/kernel/drivers/video/ti81xx/vpss/v
pss.ko i2c_mode=1
VPSS_FVID2: M3 firmware version 0x1000144 is newer,driver may not work properly.
root@dm816x-evm:~# insmod /lib/modules/2.6.37/kernel/drivers/video/ti81xx/ti81xx
fb/ti81xxfb.ko vram=0:40M,1:1M,2:1M
root@dm816x-evm:~# insmod /lib/modules/2.6.37/kernel/drivers/video/ti81xx/ti81xx
hdmi/ti81xxhdmi.ko
HDMI W1 rev 2.0
HDMI CEC Spec version 1.2
I2C No Ack
root@dm816x-evm:~# insmod /lib/modules/2.6.37/kernel/drivers/media/video/ti81xx/
ti81xxvo.ko
root@dm816x-evm:~# insmod /lib/modules/2.6.37/kernel/drivers/media/video/tvp5150
.ko
root@dm816x-evm:~# insmod /lib/modules/2.6.37/kernel/drivers/media/video/ti81xx/
ti81xxvin.ko
ti81xxvin ti81xxvin: Error registering v4l2 subdevice
root@dm816x-evm:~#
root@dm816x-evm:~#
root@dm816x-evm:~#
root@dm816x-evm:~#
root@dm816x-evm:~# echo 0 > /sys/devices/platform/vpss/graphics0/enabled
VPSS_GRPX : please open fb0 node first.
root@dm816x-evm:~# ./saLoopBack
failed to open capture device
Error in opening capture device for channel 0
root@dm816x-evm:~#
Please help me in clearing this error.
Thanks and Regards
Ajna