Hai Im sekra
I'm using Beagleboard XM based custom board.when i ready to boot the android on my device it doesn't shows up anything on the display expert the backlight.(nothing on the display)
Note:The logo is not follows up,LCD is blank
Error::
Freeing init memory: 208K
init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj inste.
init: cannot open '/initlogo.rle'
init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
/system/bin/sh: No controlling tty (open /dev/tty: No such device or address)
/system/bin/sh: warning: won't have full job control
enabling adb
adb_open
root@android:/ # init: untracked pid 1040 exited
init: untracked pid 1114 exited