This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem in android INIT file



Hai i'm Sekra.I'm using ANDROID ICS right now for my beagleboard xm based custom board using OMAP3.

I compiled the MLO,uboot,uImage,rootfs in my ics source for my own.all were working file but INIT file shows problem i think.i didn't know what does happens.i posted the error below

*******************************************************************************************************************

mmcblk0: mmc0:59b4 00000 7.34 GiB

mmcblk0: p1 p2 p3

EXT3-fs (mmcblk0p2): error: couldn't mount because of unsupported optional features (240)
EXT2-fs (mmcblk0p2): error: couldn't mount because of unsupported optional features (240)
EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
VFS: Mounted root (ext4 filesystem) on device 179:2.
Freeing init memory: 208K
init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead.
init: cannot open '/initlogo.rle'
init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
enabling adb
adb_open
/system/bin/sh: No controlling tty (open /dev/tty: No such device or address)
/system/bin/sh: warning: won't have full job control
root@android:/ #

init: untracked pid 1041 exited
init: untracked pid 1106 exited
init: untracked pid 1127 exited
init: untracked pid 1120 exited
init: untracked pid 1132 exited

I didn't know what s the problem.i you guess anything reply me....Thanks in advance