Iam using EZSDK_5_05_02_00 version of the source for DM8168 processor. By default the code supports TVP7002 video decoder for capturing the video data. We are using ADV7182 decoder instead of 7002 chip. Is there any driver available for ADV7182.
Currently the linux driver is available for adv7180. Can i use the same driver for adv7182, or any changes i need to do for porting from 7180 to 7182 driver?
If there is no driver what all changes I should do for porting the video encoder?