This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

REG Driving Low a non GPIO pin

Hi,

The problem iam facing is that i need to configure pins which need to drive low to activate few pins of NAND (which are active low like NAND_WE, NAND_WRITE,NAND_NCS0,NAND_OE) these are to be configure using standard pins not GPIO's. 

Can i drive low these pins in some way. if it is GPIO its easier for me and i can do it using the GPIOPinWrite(). But i need to follow my custom schematic. can i do the same for dedicated pins (other than GPIO config in mode 7)?

Regards,

Shradhanand