I am attempting to use a higher resolution (800x480) lcd panel with the AM335x Starter Kit. This new LCD requires some configuration over SPI. I would like to know the best way to do this. I am using the latest Rowboat build of Android.
I have made an adapter board that connects all of the display pins on J1 and the SPI pins on J11 (the zigbee header) to the new display.
From my understanding I now need to do the following:
- Edit the "NHD-4.3-ATXI#-T-1" panel in /kernel/drivers/video/da8xx-fb.c with the correct timing/resolution values.
- Set the pinmux for the SPI pins on J11 and configure spidev. (Referring to this post. http://e2e.ti.com/support/arm/sitara_arm/f/791/t/218851.aspx)
- Set the control registers on the LCD over the SPI
Does that sound reasonable? Is there a specific place I should stick the SPI writes?