This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Create root filesystem tarball

Hi,

I try to create the rootFs tarball according to TI-Android-ICS-4.0.3-DevKit-3.0.1 DeveloperGuide.

According to the instruction:

  make TARGET_PRODUCT=<product name> fs_tarball</code>
Q1: what the meaning of </code>?
when i try the command without the </code>, i got the following errors:

gabi@gabi-VirtualBox:~/rowboat-android/TI-Android-ICS-4.0.3_AM335x_3.0.1$ make TARGET_PRODUCT=am335xevm fs_tarball
============================================
PLATFORM_VERSION_CODENAME=REL
PLATFORM_VERSION=4.0.3
TARGET_PRODUCT=am335xevm
TARGET_BUILD_VARIANT=eng
TARGET_BUILD_TYPE=release
TARGET_BUILD_APPS=
TARGET_ARCH=arm
TARGET_ARCH_VARIANT=armv7-a-neon
HOST_ARCH=x86
HOST_OS=linux
HOST_BUILD_TYPE=release
BUILD_ID=IML74K
============================================
rm -rf /home/gabi/rowboat-android/TI-Android-ICS-4.0.3_AM335x_3.0.1/out/target/product/am335xevm/android_rootfs
mkdir /home/gabi/rowboat-android/TI-Android-ICS-4.0.3_AM335x_3.0.1/out/target/product/am335xevm/android_rootfs
cp -r /home/gabi/rowboat-android/TI-Android-ICS-4.0.3_AM335x_3.0.1/out/target/product/am335xevm/root/* /home/gabi/rowboat-android/TI-Android-ICS-4.0.3_AM335x_3.0.1/out/target/product/am335xevm/android_rootfs
cp: cannot stat `/home/gabi/rowboat-android/TI-Android-ICS-4.0.3_AM335x_3.0.1/out/target/product/am335xevm/root/*': No such file or directory
make: *** [fs_tarball] Error 1

Help!

thnaks

Gabi

  • Hi Gabi,

    Please follow below commands to build Android sources and create a rootfs tarball.
    Build Android sources:
    $ make TARGET_PRODUCT=am335xevm OMAPES=4.x 
    Create rootfs tarball:
    $ make TARGET_PRODUCT=am335xevm OMAPES=4.x fs_tarball

    Regards,
    Pankaj
  • Hi,

    i'm stuck in something.
    After giving "make TARGET_PRODUCT=am335xevm_sk OMAPES=4.x" command i get the following logs.
    Doyou have an idea what could be the problem?


    mehmet@kickoff:~/TI_Android_JB_4.2.2_DevKit_4.1.2$ make TARGET_PRODUCT=am335xevm_sk OMAPES=4.x
    ============================================
    PLATFORM_VERSION_CODENAME=REL
    PLATFORM_VERSION=4.2.2
    TARGET_PRODUCT=am335xevm_sk
    TARGET_BUILD_VARIANT=eng
    TARGET_BUILD_TYPE=release
    TARGET_BUILD_APPS=
    TARGET_ARCH=arm
    TARGET_ARCH_VARIANT=armv7-a-neon
    HOST_ARCH=x86
    HOST_OS=linux
    HOST_OS_EXTRA=Linux-3.13.0-48-generic-x86_64-with-Ubuntu-14.04-trusty
    HOST_BUILD_TYPE=release
    BUILD_ID=JDQ39
    OUT_DIR=out
    ============================================
    find: `src': No such file or directory
    PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/Effect_Tick.ogg:system/media/audio/ui/Effect_Tick.ogg ignored.
    PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/KeypressStandard.ogg:system/media/audio/ui/KeypressStandard.ogg ignored.
    PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/KeypressSpacebar.ogg:system/media/audio/ui/KeypressSpacebar.ogg ignored.
    PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/KeypressDelete.ogg:system/media/audio/ui/KeypressDelete.ogg ignored.
    PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/KeypressReturn.ogg:system/media/audio/ui/KeypressReturn.ogg ignored.
    PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/VideoRecord.ogg:system/media/audio/ui/VideoRecord.ogg ignored.
    PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/camera_click.ogg:system/media/audio/ui/camera_click.ogg ignored.
    PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/LowBattery.ogg:system/media/audio/ui/LowBattery.ogg ignored.
    PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/Dock.ogg:system/media/audio/ui/Dock.ogg ignored.
    PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/Undock.ogg:system/media/audio/ui/Undock.ogg ignored.
    PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/Lock.ogg:system/media/audio/ui/Lock.ogg ignored.
    PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/Unlock.ogg:system/media/audio/ui/Unlock.ogg ignored.
    PRODUCT_COPY_FILES frameworks/base/data/sounds/ringtones/ogg/Sceptrum.ogg:system/media/audio/ringtones/Sceptrum.ogg ignored.
    PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/KeypressStandard_120.ogg:system/media/audio/ui/KeypressStandard.ogg ignored.
    PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/KeypressSpacebar_120.ogg:system/media/audio/ui/KeypressSpacebar.ogg ignored.
    PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/KeypressDelete_120.ogg:system/media/audio/ui/KeypressDelete.ogg ignored.
    PRODUCT_COPY_FILES frameworks/base/data/sounds/effects/ogg/KeypressReturn_120.ogg:system/media/audio/ui/KeypressReturn.ogg ignored.
    PRODUCT_COPY_FILES frameworks/base/data/sounds/notifications/ogg/Capella.ogg:system/media/audio/notifications/Capella.ogg ignored.
  • Hi,

    Only the latest release JB4.2.2 is supported in this forum on BeagleBone Black and other AM335x platforms. Sorry for the inconvenience.