This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EMIF Speed Decrease



Hey guys,

So a customer is trying to fab a bunch of boards with Sitara on them. However, he has only qual'd a previous silicon revision of Sitara (May 2012 data sheet) on his board that ran the EMIF clock at 606MHz. The new silicon revision (v2.1) according to the April 2013 datasheet online runs the EMIF clock now at 800 MHz, not 606MHz.

If he dropped the new silicon revision of Sitara onto his circuit board with the faster EMIF (800MHz), would he have any problems (with/without dialing down the clock to 606MHz)?

He doesn't care about speed at this point and is primarily concerned that he doesn't waste the money to FAB a bunch of boards using the new revision of Sitara, just to find out that they don't work after the fact.

I would appreciate any assistance that can point me in the right direction on this issue!

 

Thanks,

Sean