This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Early suspend on OMAP4430

Hi,

We have ported Android JB 4.2.5P1 onto our custom board based on OMAP4430.

The current measured on our board during on-state is around 250mA. However when the board goes to early suspend the current on the board rises and measures around 300mA, which is strange because ideally the current should reduce due to the display going off during early suspend. During complete suspend the current measured is 10mA, which is working fine. There seems to be a problem during early suspend.

Could someone help us on this ?

Thank You

Prakash