Hi all ,
This is second post about the same propose ,
I want to connect between tow TMDSEVM6670LE boards (Board_1 as TX and Board_2 as RX) via Ethernet cable (by attaching each end of this cable with the Ethernet port of each board ) ,
I used the example which is in the directory :
C\ProgramFiles\TexasInstruments\pdk_C6670_1_0_0_17\packages\ti\drv\exampleProjects\PA_emacExample_exampleProject
Can i do this propose using this example ?
if yes :
I am read a lot of posts related to using this example and there is no specific steps to do my propose .
Can any one help me ?
Thanks in Advanced ,
Muhammad