Hi All,
As the OMAP-138 EVM use ti-dvsdk_omapl138-evm_04_03_00_06 and it have lot of example special for the DSPLINK example is very interesting for us, but when i tried to load ti-dvsdk_omapl138-evm_04_03_00_06 to my LCDK board, it is hangup on booting image as this post shows http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/t/211004.aspx.
So, my question is does any one success use dvsdk_omapl138-evm compiled kernel to booting up LCDK board? or i need to change something to get it working.
Thank you very much