Hi,
I will be using the TMS320C6748BZWTD4 with a core voltage of 1.3V.
I won't be using the USB port but from the datasheet it looks like I still need to connect USB_CVDD to 1.2V. 1.2V will also be connected to filters on the PLL_VDDA and PLL_VSSA lines.
1.2V will not be used anywhere else on my board.
Could you give me an indication of the current that will be required for these 1.2V connections?
I've seen that the maximum operating conditions for these supplies is -0.5V to 1.4V but the recommended operating voltage is 1.14 to 1.32V. I'm assuming that I can't connect them directly to the 1.3V supply which has a recommended tolerance of 1.25V to 1.35V.
Thanks, Amanda