This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

McASP and serializer initialization question

I am using EZSDK version 5.05.02.00 with the DM8168 processor on the Spectrum Digital DM8168 EVM.

In arch/arm/mach-omap2/board-ti8168evm.c I believe I see where the serializer directions are configured.

static u8 ti8168_iis_serializer_direction[] = {
TX_MODE, RX_MODE, INACTIVE_MODE, INACTIVE_MODE,
INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE,
INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE,
INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE,
};

My interpretation of this is that AXR0 (position 0 in the data structure) is being configured as a transmitter and that AXR1 (position 1 in the data structure) is being configured as a receiver.  Could someone please confirm that I am interpreting this correctly?

Per the TI81xx PSP Porting Guide and the "ALSA Framework Hookup" section

http://processors.wiki.ti.com/index.php/TI81xx_PSP_Porting_Guide#ALSA_framework_hookup

I see that the association between the codec and the McASP instance being used is via the number used in the cpu_dai_name.

Where/how is the association made between the serializer channels (AXR0, AXR1) and the capture or playback data paths?