Can any one tell me does the OMAP 3525 & 3530 support these register which is not available on its Datasheet.
PRM_VP1_CONFIG 0x4830 72B0
PRM_VP1_VSTEPMIN 0x4830 72B4
PRM_VP1_VSTEPMAX 0x4830 72B8
PRM_VP1_VLIMITTO 0x4830 72BC
PRM_VP1_VOLTAGE 0x4830 72C0
PRM_VP1_STATUS 0x4830 72C4
PRM_VP2_CONFIG 0x4830 72D0
PRM_VP2_VSTEPMIN 0x4830 72D4
PRM_VP2_VSTEPMAX 0x4830 72D8
PRM_VP2_VLIMITTO 0x4830 72DC
PRM_VP2_VOLTAGE 0x4830 72E0
PRM_VP2_STATUS 0x4830 72E4
I got the above register details from OMAP3430 Linux Code which we got along with our Logic PD Zoom Kit & these registers are used for configuring Smart reflex. If so can any one provide me details about those registers & usage information?
In the PRCM datasheet sprufa5a I couldn’t able to access the following chapters.
Basic Programming Model
· Voltage Processor Initialization Basic Programming Model : [21] [22] [23] [24] [25] [26] [27] [28] [29] [30] [31] [32]
· Changing OPP Using the SmartReflex Module : [33]
· Changing OPP Using Only the Voltage Processor Module : [34]
Use Cases and Tips
· DVFS Using SmartReflex : [36] [37] [38] [39]
Kindly provide me the details.