I have a question on timing related to the EMIFA while in Asynchronous Select Strobe Mode during a read operation.
The OMAP datasheet at Table 5-24 item NO. 10 tw(EMOEL) says that the min can be (RST)*E-3 (ns).
Does this mean that EMA_OE# can go away 3ns sooner than the rising edge of EMA_CLk?
(If this is true, then we have to make sure our data being read is available 3ns after OE rises.)
If this does not account for the “-3ns”, then where does it come from?