This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Differences between 8168 ES1.1 and ES2.1 CPU revision?

Hi all,

I have two DM8168 TI EVMs that I'm developing on. One of them is Rev G and the other is Rev J. According to http://support.spectrumdigital.com/boards/evm816x/revg/files/evm816x_faq.htm the main difference between the two revisions is the upgrade from CPU revision 1.1 to 2.1.

I have a usecase that connects a NULL source to the display. This usecase works nicely on the Rev G board, but hangs on the Rev J board.

Another thing I've noticed is that the boot log prints "UNKNOWN CPU detected, defaulting to VPS_PLATFORM_CPU_REV_2_0" for the Rev J board.

Is the 2.1 revision not supported?

I'm using the DVR RDK 3.5 for this.

Thanks,
Philipp