Other Parts Discussed in Thread: OMAP-L138, OMAPL138, 66AK2H12
I have a prototype application running on the ADSP-21469-EZBOARD. The application is using 90% of available FIR resources, including the FIR accelerator.
AD doesn´t offer code protection, so I am looking at the C6748 which has secure boot. Is secure boot only available for C6748?
Will the C6748 match the ADSP-21469 regarding FIR performance?
I have tried to verify that the C6748 (or OMAP-L138) can handle three I2S input channels and four i2S output channels at 192 kbit/s using the one McASP port. I believe that it is possible but would like to have this confirmed. Is there a difference between C6748 and OMAP-L138 regarding McASP wires available?
I need a development board with all McASP pins available on an expansion header (or a good 6/8 channel audio codec on board). I have found the Zoom™ OMAP-L138 EVM, but it isn't clear if the McASP pins are available. Any suggestions appreciated.
Mårten