Other Parts Discussed in Thread: DA8XX
Hello,
I was just wanting some assistance with the Beaglebone Black image of Android, which is available from here:
This image works correctly. I have a 4DCAPE-43T CAPE from 4D Systems which works well, however the prototype 4DCAPE-70T CAPE does not display at all. The CAPE is based on the latest revision LCD7 cape from CircuitCo, so I wonder if this image has the same sort of problem as the LCD7 cape too?
I was just wanting to know if there was any chance the image could be updated to allow the 7" CAPES to function correctly? It is currently just a blank screen.
On a seperate note, I have been discussing the Android 4.2.2 image with Andrew Henderson from here:
http://icculus.org/~hendersa/android/
He has a 4.2.2 image which uses the 3.8 Kernel. As I understand it, the TI image uses the 3.2 Kernel. One downside to Andrews image is it doesnt use hardware acceleration for the GPU like the TI image does, so it is all in software and is therefore slower, however since it uses the later 3.8 kernel it allows the use of more Capes, access to the device tree to configure SPI/UARTS/I2C etc which the 3.2 kernel I believe does not allow. This makes it more usable for users who wish to 'do' more 'stuff' with Android and other devices.
I am just wondering if TI is still developing this, and if the image will be going to 3.8 at all, while still maintaining the hardware accelerated GPU features it has currently, and also bringing in compatibility for the 7" LCD CAPES?
I have been in touch with Tyler Berryhill and Mark Easley from TI, who pointed me over to this forum.
I am not linux expert myself by any means.
Kind Regards
James