Other Parts Discussed in Thread: OMAP3530
I have recently been using a OMAP3530 EVM in a ethernet/IP forwarding mode. All is working OK with small low data rate pings, however when I start streaming video Packets(UDP) the incoming Ethernet port on the OMAP3530EVM starts to drop a lot of the udp packets. MTU is set at 1500 and I am only sending <1Mbps data stream. The OMAP is clearly not CPU limited, and the ethernet should also be able to easily handle this data rate.
Does anyone know what the default Ethernet configuration is with the TI DVSDK dvsdk_3_00_01_42? 10Mbps? Full or Half duplex?
Is there a utility available for seeing what the configuration is? or for more info on why the connection is dropping packets?
Thanks for any insight.
-Simon