This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

camera sensor MT9v022 with OMAP L138

Other Parts Discussed in Thread: OMAP-L138, OMAPL138, PMP, DA8XX

Hi,

I interface the Omap-L138 with MT9V022 camera module. I facing some issues when interfacing the camera and the Omap-L138.

I have attached the log  below for your reference. Please find it.

I added  I2C_BOARD_INFO("mt9v022", 0x48),  in  board-omapl138-hawk.c

 

static struct i2c_board_info __initdata omapl138_hawk_i2c_devices[] = {

{

I2C_BOARD_INFO("mt9v022", 0x48),

},

}; 

Issues in log:

mt9v022 1-0048: MT9V022: missing soc-camera data!

mt9v022: probe of 1-0048 failed with error -22

 

I have anything(platform data or ?) to add in  board-omapl138-hawk.c .

And how to add the platform data for MT9V022 in  board-omapl138-hawk.c.

Kindly give any suggestion for this problem.

LOG:


NAND:
NAND device: Manufacturer ID: 0x01, Chip ID: 0xd3 (AMD NAND 1GiB 3,3V 8-bit)
NAND bus width 16 instead 8 bit
1024 MiB
MMC: davinci: 0
** Warning - bad CRC, using default environment

In: serial
Out: serial
Err: serial
ARM Clock : 300000000 Hz
DDR Clock : 150000000 Hz
Net: Ethernet PHY: GENERIC @ 0x07
DaVinci-EMAC
Hit any key to stop autoboot: 0
reading boot.scr

** Unable to read "boot.scr" from mmc 0:1 **
reading uImage

2253004 bytes read
## Booting kernel from Legacy Image at c0700000 ...
Image Name: Linux-3.1.10
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2252940 Bytes = 2.1 MiB
Load Address: c0008000
Entry Point: c0008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
Linux version 3.1.10 (marudham@marudham-Compaq-420) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #1 PREEMPT Wed Sep 18 17:24:55 IST 2013
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
CPU: VIVT data cache, VIVT instruction cache
Machine: AM18x/OMAP-L138 LCDK
Memory policy: ECC disabled, Data cache writeback
DaVinci da850/omap-l138/am18x variant 0x1
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 32512
Kernel command line: console=ttyS2,115200n8 root=/dev/mmcblk0p2 rw rootwait ip=off
PID hash table entries: 512 (order: -1, 2048 bytes)
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 128MB = 128MB total
Memory: 125408k/125408k available, 5664k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xff000000 - 0xffe00000 ( 14 MB)
vmalloc : 0xc8800000 - 0xfea00000 ( 866 MB)
lowmem : 0xc0000000 - 0xc8000000 ( 128 MB)
modules : 0xbf000000 - 0xc0000000 ( 16 MB)
.text : 0xc0008000 - 0xc03fbefc (4048 kB)
.init : 0xc03fc000 - 0xc041e000 ( 136 kB)
.data : 0xc041e000 - 0xc044a4c0 ( 178 kB)
.bss : 0xc044a4e4 - 0xc0464f1c ( 107 kB)
SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Preemptible hierarchical RCU implementation.
NR_IRQS:245
Console: colour dummy device 80x30
Calibrating delay loop... 148.88 BogoMIPS (lpj=744448)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
DaVinci: 144 gpio irqs
NET: Registered protocol family 16
EMAC: MII PHY configured
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
Advanced Linux Sound Architecture Driver Version 1.0.24.
Switching to clocksource timer0_1
Switched to NOHz mode on CPU #0
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
msgmni has been set to 244
io scheduler noop registered (default)
Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO 0x1c42000 (irq = 25) is a 16550A
serial8250.0: ttyS1 at MMIO 0x1d0c000 (irq = 53) is a 16550A
serial8250.0: ttyS2 at MMIO 0x1d0d000 (irq = 61) is a 16550A
console [ttyS2] enabled
brd: module loaded
ahci ahci: forcing PORTS_IMPL to 0x1
ahci ahci: AHCI 0001.0100 32 slots 1 ports 3 Gbps 0x1 impl platform mode
ahci ahci: flags: ncq sntf pm led clo only pmp pio slum part ccc
scsi0 : ahci_platform
ata1: SATA max UDMA/133 mmio [mem 0x01e18000-0x01e19fff] port 0x100 irq 67
davinci_mdio davinci_mdio.0: davinci mdio revision 1.5
davinci_mdio davinci_mdio.0: detected phy mask ffffff7f
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[7]: device 0:07, driver unknown
ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
ohci ohci.0: DA8xx OHCI
ohci ohci.0: new USB bus registered, assigned bus number 1
Waiting for USB PHY clock good...
ohci ohci.0: irq 59, io mem 0x01e25000
usb usb1: New USB device found, idVendor=1d6b, idProduct=0001
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: DA8xx OHCI
usb usb1: Manufacturer: Linux 3.1.10 ohci_hcd
usb usb1: SerialNumber: ohci.0
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
omap_rtc: RTC power up reset detected
i2c /dev entries driver
lirc_dev: IR Remote Control driver registered, major 253
IR NEC protocol handler initialized
IR RC5(x) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR RC5 (streamzap) protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
IR LIRC bridge handler initialized
Linux video capture interface: v2.00
mt9v022 1-0048: MT9V022: missing soc-camera data!
mt9v022: probe of 1-0048 failed with error -22
gspca: v2.13.0 registered
vpfe_init
usbcore: registered new interface driver uvcvideo
USB Video Class driver (1.1.1)
davinci_mmc davinci_mmc.0: Using DMA, 4-bit mode
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
ALSA device list:
No soundcards found.
TCP cubic registered
NET: Registered protocol family 17
davinci_emac davinci_emac.1: using random MAC addr: 42:d0:69:6a:19:3b
console [netcon0] enabled
ata1: SATA link down (SStatus 0 SControl 300)
netconsole: network logging started
omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
Waiting for root device /dev/mmcblk0p2...
mmc0: new SD card at address 1234
mmcblk0: mmc0:1234 SA02G 1.83 GiB
mmcblk0: p1 p2
kjournald starting. Commit interval 5 seconds
EXT3-fs (mmcblk0p2): using internal journal
EXT3-fs (mmcblk0p2): recovery complete
EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode
VFS: Mounted root (ext3 filesystem) on device 179:2.
Freeing init memory: 136K
INIT: version 2.86 booting
Please wait: booting...
Error opening /dev/fb0: No such device or address
Starting udev
udevd (1015): /proc/1015/oom_adj is deprecated, please use /proc/1015/oom_score_adj instead.
udev: starting version 141
Remounting root file system...
Caching udev devnodes
Populating dev cachemv: cannot rename '/tmp/devices': No such file or directory
NET: Registered protocol family 10
ALSA: Restoring mixer settings...
Configuring network interfaces... /usr/sbin/alsactl: load_state:1625: No soundcards found...
davinci_mdio davinci_mdio.0: resetting idled controller
net eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:07, id=7c0f1)
ADDRCONF(NETDEV_UP): eth0: link is not ready
eth0 no wireless extensions.

udhcpc (v1.13.2) started
Sending discover...
Sending discover...
Sending discover...
No lease, forking to background
done.
Setting up IP spoofing protection: rp_filter.
Tue Apr 10 20:33:00 UTC 2012
INIT: Entering runlevel: 5
Starting system message bus: dbus.
Starting Hardware abstraction layer hald
Starting Dropbear SSH server: dropbear.
Starting telnet daemon.
Starting network benchmark server: netserver.
Starting syslogd/klogd: done
Starting thttpd.
Starting Lighttpd Web Server: lighttpd.
2012-04-10 20:33:09: (log.c.166) server started
/
Starting Matrix GUI applicationinsmod: can't read '/lab1/armuga/driver/csscanner_fx2.ko': No such file or directory
insmod: can't read '/lab1/armuga/driver/csscanner_main.ko': No such file or directory
.
***************************************************************
***************************************************************
NOTICE: This file system contains the followin GPLv3 packages:
binutils-symlinks
binutils
gdbserver

If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above

NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************

_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|

Arago Project http://arago-project.org omapl138-lcdk ttyS2

Arago 2011.09 omapl138-lcdk ttyS2

omapl138-lcdk login: