Hi,
The Gain and Offset errors are specified as 'Nominal' in Datasheet Table 3-17. TSC_ADC Electrical Parameters.
-What are these values as 'Maximum' over temp and process?
Thanks.
/Magnus Aman
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Biser,
Please answer the question without 'should' or 'would' please.
Let me rephrase it:
-Given that these errors are following a normal distribution over devices and their operating specs, can you confirm that the magnitude of them (+/- 2LSB) correspond to the 6-sigma limits, as defined by
http://en.wikipedia.org/wiki/Six_Sigma#Origin_and_meaning_of_the_term_.22six_sigma_process.22
Our analog parts Min/Max values are often based on 6-sigma.
-We would like to know the probability that the errors are greater than the specified +/-2 LSB.
For 6-sigma that probability is <0.00034%.
Thanks again.
/Magnus Aman
The maximum values for these parameters are not published in the data sheet because they are not measured on every device as part of the standard production test flow. Not testing these parameters reduces test time and allows TI to offer a lower cost product to our customers.
Regards,
Paul