Other Parts Discussed in Thread: OMAP3530
Using Texas Instruments' EVMFlash 3530 utility for Micron memory (v1.2.1.0), I have tried to download the TIEVM3530-nand.raw image file to the EVM (my EVM has a Micron NAND flash). This image file is taken from the Bsquare BSP and contains both XLDR and EBOOT images.
I have set the EVMFlash download as instructed in the BSP user's guide (UART port:1, baud: 115200, mode: boot rom, device type: NAND, erase entire flash, verify download). The board's DIP switch is configured appropriately (2 and 4 switches are on). The serial cable is connected to UART3, and I start the download while the board is still not powered. The message "reset target to proceed" appears. Then, I power on the board and expect the process to start, but nothing happens. The same message still appears, and no progress is marked by the EVMFlash utility.
What is missing here? I would appreciate your help.
Ishai