The am335x power on Power-Up Sequencing: 1.8V, 3.3V, 1.1V. When the device is Power-Up, the RXD of the uart will input the power (3.3V) to the am335x.So when the 1.8V is power on,the 3.3v of the am335x will have 1.0v.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When my system have many board , one board have an am335x and a power system? One board have communications to the other board. I can not ensure"Power supplies to external components must ramp-up after the Am335x power supplies."
There is a good chance your system will violate the AM335x Absolute Maximum Ratings parameter "Steady State Max. Voltage at all IO pins" if you do not properly sequence your power supplies.
There is also a chance you will violate a similar parameter for the peripheral devices attached to AM335x since most CMOS devices have a similar limit. In a few cases, devices may be designed with fail-safe inputs which allow voltage to be applied to the input while the device is powered off.
This is one of the small design details that is commonly over-looked, but power sequencing of all devices in a system should be considered when designing your product.
In some cases, it may be necessary to put isolation circuits that disconnect devices while power is sequenced
Regards,
Paul
I move the other board from the system, the Power-Up Sequencing and Power-Down Sequencing is a above.
Are three any problems?
ALL the below 1.1V of the am335x are connect together.
ALL the below 1.8V of the am335x are connect together.
ALL the below 3.3 of the am335x are connect together.
vdd_core 1.1
vdd_mpu 1.1
vdds_pll_mpu 1.8
vdds_sram_mpu_bb 1.8
vdds_sram_core_bg 1.8
vdda3p3v_usb0 vdda3p3v_usb1: 3.3
vdda1p8v_usb0 vdda1p8v_usb0:1.8
vdds_pll_ddr 1.8
vdds_ddr 1.8
vddshvx 3.3
vdds 1.8
vdda_adc : 10k to gnd
vdds_adc gnd
vpp: no connect
vdds_pll_core_lcd 1.8
vdds_rtc 1.8
cap_vdd_rtc 1.1
RTC_KALDO_ENn:10k to 1.8
VDDS_OSC: 1.8