Other Parts Discussed in Thread: OMAP-L138
I'm working with the OMAP-L138 eXperimenter kit from Logic PD. It comes with a SDRAM connected via the "DDR2 Memory Controller" EMIF but I'm still unsure how this interface is being driven, as it does not seem to be driven with a Linux driver. How is this interface driven?
I'm also looking into connecting a NOR or NAND flash to the EMIFA port, and I'm wondering how this can be driven. Would I need a Linux driver for this or can I use a similar approach to what is currently being done to drive the DDR Mem Controller EMIF? Please advice.