This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ecat_appl project, comfort configuration

Hello,

I am working on Am335x TI ICE board for a ethercat project. I am using the example code: ie. ecat_appl project (sdk_1.1.0.1) and debuging, flashing it in 0x2000 area (using Jtag + CCS 5.4.0) with success.

As Shown in different Post, after Build, to debug ie_cat code I operate manually as follow:

I launch the Selected configuration.

I select Cortex A8, and I connect the target (this operation lauch the initialisation Script).

I reset the Cpu (Cpu Reset HW button)

I Load the ecat code: run, Load, Load Programm=>.out file

This method is applied with success, but I don't understand why the project configuration don't make it automatically.By using the <Debug> button ?

If I want to debug the ecat code, it's important for me to automatize these operations (reducing time spent).

I tried to modify the properties, but no effect, if I use the Debug button, it's like as the PC don't find the main() adress. An idea ?