Dear Mariana or others,
Question: I'd like to use a Seagate Momentus drive, which requires a password to access, in order to secure data on a remote embedded device. So I'm wondering if you think it would be feasible to design a little board with something on it (some kind of OMAP/?) which has only one function:
- At powerup or reboot (?) my little board would solicit a password either via text or just wait for it, over some kind of serial port
- it would then hook into the Momentus drive's SATA interface to deliver the needed password and therefore unlock the drive
- and then get the heck out of the way. Somehow I'd open-collector the SATA wires so that it wouldn't interfere with the normal SATA interface. I don't know boo about SATA at this point but if the little board could temporarily drive, it might be able to drive the interface relatively slowly and deliver this password.
Problem being that laptop manufacturers normally provice "BIOS support" to deliver that password, but I'm running an embedded device and can't find anything that will unlock the drive.
Do you have any suggestions?
Thanks,
:) Robert