Hi,
I'm using the beagle board for a project, I want to transfer some datas from the SDRAM location 0x80700000 to destination 0x80C00000 via DMA.
that is I want to transfer 50 bytes of data 0xAA from the source to the destination. I read the DMA module of the processor data sheet, in that it is explained for to transfer a image of size 240 x 160.
my case is different I want to transfer some data and not the image.
So can somebody please expain the procedure for the data transfer via DMA.