Other Parts Discussed in Thread: OMAP-L138, OMAPL138, AM3517
Hi TI experts
I use omap-l138 LCDK with linux SDK on it - no problem here. What I want to do is to connect some touch-screen/Simple LCD with external keyboard (if possible) to this board and develop some user friendly interface for my project. So my questions are :
1. Is it possible to connect any of LCD displays to LCDK? If yes, could you please recommend something, I mean part numbers or so - just as an example
2. Is it possible to use any graphic sub-system for the current Linux SDK, like Gnome ?
Any related info would be much appreciated.
Thx a lot in advance.
BR,
Dmitry