Other Parts Discussed in Thread: OMAP-L138, CCSTUDIO, OMAPL138
I just received my OMAP-L138 EVM, and tried starting up Code Composer Studio v3.3 to work with it. But Code Composer Studio v 3.3 will not start unless I have defined a target system. To define a target system I must use the Setup CCStudio v3.3 program, where I selected the most appropriate target from the list, and saved it. Then when I try now try to start Code Composer Studio v3.3, it makes the following complaint:
Unable to find an appropriate registry key for "ICEPick_C"
Target driver: C:\Program Files\CCStudio_v3.3\drivers\tixds510icepick_c.dvr
I've tried many variations on that, always with the same result. Any clues on what I should try next?
Thanks for your help.
-- Walter