Other Parts Discussed in Thread: TMS320C6748
Hi,
I'm working on a custom board with the TMS320C6748.
I've read all hardware guides that I could find and I thought it would be best to start my layout with decoupling the DSP.
But I've no idea where to start. The power and ground balls seem to be placed more or less random on the inner balls of the package and I don't see how I could combine two balls per via to make enough place for the capacitors (0402). I always get stuck at a ball/via combination which blocks a capacitor somewhere or I decouple 1V3 and 3V3, but then block any decoupling to a 1V8 ball.
Did I miss some structure in the ball assignment?
Are there some recommendations on how to start actual placing the capacitors? Or is there some guide line on which balls could share a via?
Thanks in advance.
Kind regards,
Remco Poelstra