This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Help on Am335x EVM IEEE 1588 usage with the newly released SDK 6.0 and PSP 4.06.00.11

I have noticed that the newly released (July 2013) SDK 6.0 with PSP 4.06.00.11 Ethernet driver is now supporting IEEE 1588 ( feature listed in 'AM335x-PSP 04.06.00.11 Features and Performance Guide').

My upcoming project needs to use the IEEE 1588 PTP function. 

Is there any example or guidelines on how toe use the PSP? I am planning to use two am335x evm boards to test the feature. 

Thanks.

Kevin