This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using 512MB DDR2 with OMAP-L138

I am having some problems connecting 512MBytes of DDR2 to the L138. It looks like the row/col address bus is limited to 14 bits (A0-13). That would require a sinlge x16 device since x8 devices appear to have 15 address bits (A0-14). If that is the case, currently the only x16 4Gbit parts are very expensive twin die parts.

Is there a method of connecting (2) 256MByte x8 devices of DDR2 to the L138?